2025-06-16 1:13 AM
Hello all,
I have a custom board with an STM32U5A9 mcu with an external MT25QL128 flash for TouchGFX assets.
I have a working loader for IAR Embedded workbench and I'm trying to port it to work with the STM32CubeProgrammer.
When building as a normal project - that is a minimal cubemx project with just ospi and clocks enabled and with my ospi functions it runs fine, read/write/erase the flash without any issues.
However, when I move it to the loader framework the init function crashes - I believe in a hard fault or some kind. It's difficult to tell for certain since debugging the loader is tricky.
The cube programmer only tells me "Error: Data read failure".
I realized that if I return early from the Init, no error is issued and the flash only read zeros - which makes sense because the ospi is not initialized yet.
Thus I found out that the issue so far is on HAL_OSPI_MspInit function that was generated by cubemx.
This part of the code returns 0:
__HAL_RCC_OSPIM_CLK_ENABLE();
return 0;
__HAL_RCC_OSPI1_CLK_ENABLE();but this code crashes:
__HAL_RCC_OSPIM_CLK_ENABLE();
__HAL_RCC_OSPI1_CLK_ENABLE();
return 0;the __HAL_RCC_OSPI1_CLK_ENABLE is a macro:
#define __HAL_RCC_OSPI1_CLK_ENABLE() do { \
__IO uint32_t tmpreg; \
SET_BIT(RCC->AHB2ENR2, RCC_AHB2ENR2_OCTOSPI1EN); \
/* Delay after an RCC peripheral clock enabling */ \
tmpreg = READ_BIT(RCC->AHB2ENR2, RCC_AHB2ENR2_OCTOSPI1EN); \
UNUSED(tmpreg); \
} while(0)And it is the SET_BIT line that's crashing. I don't know why.
It's not access as if I read the RCC->AHB2ENR2 it does not crash, only writing.
Does anyone have an idea what is going on here - or even how to debug this?
On a side note, when developing the IAR EWARM loader I had to increase the stack size for the loader to work, I could not find how to do that in the cubeprogrammer loader either.
Any help is much appreciated
Solved! Go to Solution.
2025-06-17 7:44 AM
Hi all,
I found the issue that I was having :)
For some reason the stm32programmer was calling the Init() function multiple times, and on the second run it crashed.
I solved the issue by testing whether the ospi was initialized or not
KeepInCompilation int Init()
{
if(READ_BIT(OCTOSPI1->CR, OCTOSPI_CR_EN)){
EnterMemoryMapMode();
return 1;
}
//perform the actual initialization
...
}
2025-06-16 7:49 PM
Make sure to clear/setup variables completely as no code is called to initialize statics.
For debugging one can use an available UART or other board hardware to output diagnostic or telemetry data.
Some of STs examples use interrupts and a vector table, so an informative HardFault_Handler might work. Similarly an Error_Handler that outputs file/line data before entering a while(1)
2025-06-16 7:51 PM
Enumerate the pins you're using, I could rebuild one of my loaders.
2025-06-17 12:10 AM
Hello,
> Enumerate the pins you're using, I could rebuild one of my loaders.
I'm using OCTOSPI1 in quad spi mode using port2 clk,ncs and io:
CLK: PF4
NCS: PI5
Data0: PI3
Data1: PI2
Data2: PI1
Data3: PF3
Micron memory type w/ device size of 24 .
2025-06-17 6:02 AM
Aren't those really OCTOSPI2? Sure you can map via OSPIM but not sure of the clock enables
This was my build as OCTOSPI2 w/OCTOSPIM
PF4:AF5 P2 CLK
PI5:AF5 P2 NCS
PI3:AF6 P2 IO0
PI2:AF6 P2 IO1
PI1:AF6 P2 IO2
PF3:AF5 P2 IO3
2025-06-17 6:15 AM
Thank you very much for this, unfortunately the issue is the same
2025-06-17 7:44 AM
Hi all,
I found the issue that I was having :)
For some reason the stm32programmer was calling the Init() function multiple times, and on the second run it crashed.
I solved the issue by testing whether the ospi was initialized or not
KeepInCompilation int Init()
{
if(READ_BIT(OCTOSPI1->CR, OCTOSPI_CR_EN)){
EnterMemoryMapMode();
return 1;
}
//perform the actual initialization
...
}