cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401 Discovery ADC tracing

paul2
Senior
Posted on July 15, 2014 at 22:16

Hi,

With the Keil qVision v5 Logic Analyzer I'm tracing (ST-Link) an single ADC value which is updated every 10 microsecond. Directly after starting the trace I get ''Trace: SW Buffer Overrun''.

Is this a ST-Link limitation or is it a configuration issue?

Thanks.

1 REPLY 1
Posted on July 16, 2014 at 00:13

The ST-LINK is hardly classed as a fast or professional debug solution. Try dropping the sample rate significantly below 100 KHz, or getting a faster pod like a JLink Ultra or ULink Pro

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..