2015-08-05 10:29 AM
Hello all,
I am using the ADC1 regular conversion or ADC1/2 dual-mode regular conversion to acquire a video signal. The dual-mode is used at higher frame rate. In both case, I am using the DMA. This part is working without a glitch.Now, I want to use the ADC3 to convert in regular mode a few other channels. I start the conversion after the video signal conversion is completed. The problem I have is that when I am using the dual-mode at higher frame rate, it seems the ADC3 is alway busy. Could you tell me if this configuration is possible?ADC1/2 regular dual-mode with DMA.ADC3 regular single conversion.Thank you #stm32f4 #adc2015-08-31 6:30 AM
Hi Keaven,
Your configuration doesn't seem to be an odd one.The problem I have is that when I am using the dual-mode at higher frame rate, it seems the ADC3 is alway busy. How exactly is ADC3 busy? Is there any error flag?Did you tried other configuration for ADC1/2 on which ADC3 is working also?When you debug your code, does it get stuck at a some level?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.