STM32F4 - Master Receive
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-04 1:45 PM
I am attempting to get an STM32F4 to receive data in Master mode. I am getting a problem where the RXNE interrupt is never tripped.
*Should this work, even if you have MISO tied to GND or 3.3V?*Do I need to do anything with the NSS in the peripheral?**Ignore the CS requirements of the slave for now. #stm32f4 #spi- Labels:
-
SPI
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-04 2:07 PM
There should be some master/slave examples in the firmware library.
You will however need to send some data to generate clocks for the slave to send data back to you. Reading SPIx->DR just reads an internal register, it does not generate any clocks.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-04 2:13 PM
If I write to the SPIx->DR, under what conditions will I get the RXNE register to be set? Let's say, I don't have a slave connected, but tie MISO to 3.3V. Should the MCU still tell me that I have received data?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-04 2:14 PM
If I write to the SPIx->DR, under what conditions will I get the RXNE register to be set? Let's say, I don't have a slave connected, but tie MISO to 3.3V. Should the MCU still tell me that I have received data?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-04 2:30 PM
The clocking in of the data occurs at the master, you should be able to control the edge/phase of the clock which MISO is sampled, but you are generating the clock, and the state of the data is of little consequence.
You should clear RXNE by reading SPIx->DR, when you send data by writing SPIx->DR, TXE should assert as the first bit leaves the master, RXNE should assert after the last bit leaves the master, and the last slave bit is clocked back.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-05 6:06 AM
Am I correct in saying that, from the Master's perspective, none of this is dependent on the CS or any NSS register?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-05 1:13 PM
As
Clive
says,
there are plenty of
http://eliaselectronics.com/stm32f4-tutorials/stm32f4-spi-tutorial/
Surelyyou've already done
but
checking
the check list
1- Enable clock for SPI and GPIO 2- Configure GPIO for alternate Function 3- Init the SPI (with std.library Spi_Init(Spibase, cfg) (cfg is the SPI config structure) 4- Init NVIC and define SPI isr handler(not mandatory) 5-Enable SPI (with std.library SPI_Cmd(Spibase, ENABLE)
It is not
necessary to configure
NSS
or
CS
(obviously
for
a simple test
without
slaves connected
) You can also checkthe
CLK pin
with an oscilloscope
when you send
a byte
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-05 1:40 PM
Thanks guys;
My original problems were twofold:The RXNE flag is delayed behind the TXE flag. I think that it should be by at least 1/2 the SCK period.Also, I found that if I stop by debugger (Keil) on the statement that checks for RXNE in the ISR, it always fails. But if I stop it after the if statement passes, then we are okay.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-05 5:55 PM
TXE should assert quite early, as the holding buffer transfers to the shift register, RXNE should assert after the last bit shifts out, delayed by 1/2 a cycle where the data clocks in against the opposite edge.
The peripheral viewer will likely read the DR and SR, resulting in the clearing of RXNEUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-06 5:50 AM
Okay, so let's say that I wanted to send out two bytes, and only view the return byte from the second tx. If I am putting tx data into the SPI-DR when TXE is set, will RXNE be already set immediately after I send the second byte? Would this cause an error where I would actually be reading the response from the first tx byte?