2018-06-13 11:03 PM
Hello,
I bought the new f746 discovery board but when i tried to compile some middlewares keil is throwing errors
Error &sharp603: 'Segger.MDK-Plus::Graphics:CORE:5.36.6': component requires valid MDK-ARM Plus or MDK-ARM Professional license
Do you provide any support to overcome this ? like serial number or something .
or which IDE do you recommend to explore all the graphics , fat, usb middlewares ?
Thanks
#stm32f7-discovery2018-06-13 11:25 PM
Hello,
we offer free Keil uVision license for STM32 microcontrollers based on Cortex-M0/+ core. For the rest, ST does not support free licenses.
is the official tool today for STM32 by ST. You may use unlimited flash size and any STM32.2018-06-14 12:17 AM
Keil can provide a temporary license for evaluation. You should contact them.
If you're not prepared to pay Keil, you can use the STemWin and FatFs packages, and examples that come with the CubeF7 and HAL libraries.