2018-06-13 6:36 AM
Hi,
I am running code to scan available devices on I2C bus by using HAL_I2C_Master_Transmit() .
scan is responding for RTC+EEPROM module and listing I2C addresses perfeclty.
Now I have I2C based optical switches on bus,but it is not being listed in scan, receiving HAL_TIMEOUT /HAL_BUSY flags.
same Optical switch is working well with Arduino.
following is my I2C initialization:
static void MX_I2C3_Init(void)
{hi2c3.Instance = I2C3;
hi2c3.Init.ClockSpeed = 100000; hi2c3.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c3.Init.OwnAddress1 = 0; hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c3.Init.OwnAddress2 = 0; hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
// MSP init:
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hi2c->Instance==I2C3) { /* USER CODE BEGIN I2C3_MspInit 0 */ __HAL_RCC_I2C3_CLK_ENABLE(); /* USER CODE END I2C3_MspInit 0 */ /**I2C3 GPIO Configuration PC9 ------> I2C3_SDA PA8 ------> I2C3_SCL */ GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_OD; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_I2C3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_I2C3; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* Peripheral clock enable */
/* USER CODE BEGIN I2C3_MspInit 1 */
/* USER CODE END I2C3_MspInit 1 */
}}
I am using STM32F207ZG nulcleo board for development and STM32Cube_FW_F2_V1.6.0 SDK.
Seeking help in resolving this issue...
Thanks.
2018-06-13 4:10 PM
I cannot simulate your issue, but please consider;
How long is the data trace on your board ? no more than 100mm I hope.
You may need to lower the pullup value, maybe 1k pullups on SDA and SCLK
You may need to lower the clocking rate.
You may have a bug with the addressing of the errant parts.
2018-06-13 4:17 PM
not sure why you'd use master_transmit to scan the bus
here's my i2c bus scan code:
printf('Scanning I2C bus:\r\n');
HAL_StatusTypeDef result;uint8_t i;for (i=1; i<128; i++){ /* * the HAL wants a left aligned i2c address * &hi2c1 is the handle * (uint16_t)(i<<1) is the i2c address left aligned * retries 2 * timeout 2 */ result = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 2, 2); if (result != HAL_OK) // HAL_ERROR or HAL_BUSY or HAL_TIMEOUT { printf('.'); // No ACK received at that address } if (result == HAL_OK) { printf('0x%X ', i); // Received an ACK at that address }}printf('\r\n');2018-06-14 12:07 AM
Previously I tried with
HAL_I2C_IsDeviceReady(), but same results were coming. In Description I found that
HAL_I2C_IsDeviceReady() is only for memory devices so I moved for master_transmit.
2018-06-14 12:23 AM
I am having STM32F2 nucleo board, SDA- SCL lines are having 2.2k pullups....
Clock is at 100kHz but still not getting desired output with STM controller..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.