2015-08-19 1:41 AM
Hello there,
I am trying to find any resources on how to emulate eeprom inside flash of an STM32F4 MCU using the HAL library, but I cannot find anything. Could anyone please point me out any resources, examples or tutorials? Also, what are those in stm32_hal_legacy.h, i dont get it:/** @defgroup HAL_FLASH_Aliased_Functions HAL FLASH Aliased Functions maintained for legacy purpose
* @{ */ &sharpdefine FLASH_HalfPageProgram HAL_FLASHEx_HalfPageProgram &sharpdefine FLASH_EnableRunPowerDown HAL_FLASHEx_EnableRunPowerDown &sharpdefine FLASH_DisableRunPowerDown HAL_FLASHEx_DisableRunPowerDown &sharpdefine HAL_DATA_EEPROMEx_Unlock HAL_FLASHEx_DATAEEPROM_Unlock &sharpdefine HAL_DATA_EEPROMEx_Lock HAL_FLASHEx_DATAEEPROM_Lock &sharpdefine HAL_DATA_EEPROMEx_Erase HAL_FLASHEx_DATAEEPROM_Erase &sharpdefine HAL_DATA_EEPROMEx_Program HAL_FLASHEx_DATAEEPROM_Program #eeprom #flash2015-08-19 2:02 AM
Here you have an example with the ''old'' spl library's http://www.st.com/web/en/catalog/tools/PF257902#.
2015-08-19 4:26 AM
Hi Bremen,
There is an application note that provides the EEPROM emulation driver ( and its associatedhttp://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257902
).But it is not developed based on HAL drivers.Regarding the file stm32_hal_legacy.h, it was added in order to let the migration from one STM32CubeF4 version to another easier for variables that were renamed in the aim of having compatible Cube packages independent of the used family.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-09-09 11:20 PM
Are there any HAL examples for this? Does HAL lib even support this?
2018-01-27 4:22 AM
check this