STM32F4 Discovery with ADS7870 (TI) ADC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-15 1:19 AM
Hi,
I'm trying to communicate between the
http://www.ti.com/product/ADS7870
and the ST microcontroller STM32F4 Discovery evaluation board. I'm using IAR and at the moment I'm just trying to read register 31 from the ADC (which should return a 1) but with no luck.I'm setting the SPI on the microcontrontroller as follows: data transmitted as MSB first, clock low in idle state, data is captured on rising edge, data size is 8 bits, and full duplex transmission.
In main.c I do:
http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/3147aspx#
1
2
3
4
5
6
debug = ads7870Init();
if
(debug==1)printf
( ''adc is alive \n'' );else
printf
( ''adc is DEAD \n'' );And in
http://www.ti.com/product/ads7870
_driver.c I have:http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/3147aspx#
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
//initialize ADC
uint8_t ads7870Init( void ) {//// check ID register
if
(ads7870ReadReg(ADS7870_ID) != ADS7870_ID_VALUE)return
0;else
{
//// setup reference and buffer
ads7870WriteReg(ADS7870_REFOSC, ADS7870_REFOSC_OSCE | ADS7870_REFOSC_REFE | ADS7870_REFOSC_BUFE);
//// return success
return
1;}
}
I'm attaching a screenshot of what I see on the scope. (yellow: sclk, blue: read command register 31, purple: output from ADC).
MOSI transmits properly to the
http://www.ti.com/product/ADS7870
(the din pin receives read command), but there is no response coming from the ADC dout pin.I would really appreciate any help on this.
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-15 1:33 AM
Hi
Are you trying to communicated with the ADC immediately on STM32 boot? Bear in mind that the STM32 will boot faster than the ADC will be ready (STM32 will start booting as soon as power reaches 1.8V) What Voltage does the ADC work at? What reset circuitry is on the STM32?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-15 1:52 AM
Don't you find disturbing that your waveform doesn't match the read waveform in the ADS7870 datasheet (Fig.18)?
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-15 3:40 AM
Hi,
Can you share your init function (configuration of SPI)?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 4:10 AM
I'm using an evaluation board, so there's no reset circuitry. I'm powering the ADC from VDD on the STM32 discovery, so the power is the same for both. I'm also placing a breakpoint before the initialization of the ADS7870, so there should be enough time for this to boot.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 4:13 AM
It is the same waveform. Data is latched in the rising edge as in the datasheet.
Here is the waveform I obtain when using the ADS7870 with ATMEGA8 (where everything works properly).- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 4:17 AM
Here is my init function for the SPI:
void spi2_init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Peripheral Clock Enable -------------------------------------------------*/
/* Enable the SPI clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);
/* SPI GPIO Configuration --------------------------------------------------*/
GPIO_PinAFConfig(SPI2_MISO_MOSI_GPIO, SPI2_MISO_PIN, GPIO_AF_SPI2); //configure MISO pin
GPIO_PinAFConfig(SPI2_NSS_SCK_GPIO, SPI2_SCK_PIN, GPIO_AF_SPI2); //configure SCK pin
GPIO_PinAFConfig(SPI2_MISO_MOSI_GPIO, SPI2_MOSI_PIN, GPIO_AF_SPI2); //configure MOSI pin
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_InitStructure.GPIO_Pin = SPI2_MISO_GPIO_PIN | SPI2_MOSI_GPIO_PIN;
GPIO_Init(SPI2_MISO_MOSI_GPIO, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_InitStructure.GPIO_Pin = SPI2_SCK_GPIO_PIN;
GPIO_Init(SPI2_NSS_SCK_GPIO, &GPIO_InitStructure);
/* SPI configuration -------------------------------------------------------*/
SPI_I2S_DeInit(SPI2);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; //data captured on falling dge and clk idle is high
SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; //2.625MHz
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
/* Initializes the SPI communication */
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
/* Disable the I2S2 TXE Interrupt */
SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_TXE, DISABLE);
/* The Data transfer is performed in the SPI interrupt routine */
/* Enable the SPI peripheral */
SPI_Cmd(SPI2, ENABLE);
SPI_Init(SPI2, &SPI_InitStructure);
}
Thank you all for the help!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 4:40 AM
Hi
''Bear in mind that the STM32 will boot faster than the ADC will be ready (STM32 will start booting as soon as power reaches 1.8V)'' '' I'm also placing a breakpoint before the initialization of the ADS7870, so there should be enough time for this to boot.'' Not a good solution for you final code is it now?!? Silly question - have you tied the SS (Slave select) from STM32 to CS on the ADC? What have you done with the Reset line on the ADC? What have you done with the OscEnable line? In fact have you read the data sheet for the ADC? Pay attention to the section ''REQUIRED SUPPORT ELEMENTS''- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 4:58 AM
>> Don't you find disturbing that your waveform doesn't match the read waveform in the ADS7870 datasheet (Fig.18)?
> It is the same waveform. No, it is not. The datasheet figure shows the command LSB first, yours is MSB first. Meantime, reading the datasheet revealed, that it features both, and MSB first is the default. A cunning way to mislead the casual reader... Also, you don't show the /CS signal. The description in the datasheet indicates, that it's important to have a low-going transition on /CS before start of communication. There is an alternative procedure described on the bottom of page 17. > Data is latched in the rising edge as in the datasheet. But that's only if the RISE/FALL pin is tied to 1. How is it in your circuit?> Here is the waveform I obtain when using the ADS7870 with ATMEGA8 (where everything works properly).
Then what are the differences between these two cases? JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 5:03 AM
One more thing - the waveform you presented above exhibits significant ringing on the edges. If these are real and not only artifacts of improper measurement setup, they may be seen by the SPI receiver in the ADC as false clocks and throw the receiver out of sync.
JW