2014-06-01 7:16 PM
Hello,
I'm using STM32F4 discovery to develop usart communication function. The usart parameter is below./// Set serial port
USART_StructInit(&USART_InitStructure); USART_InitStructure.USART_BaudRate = 9600; ///< 9600bps USART_InitStructure.USART_WordLength = USART_WordLength_9b; ///< data 8bit + parity 1bit USART_InitStructure.USART_StopBits = USART_StopBits_1; ///< stop 1bit USART_InitStructure.USART_Parity = USART_Parity_Even; ///< parity even USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; ///< enable Rx, Tx USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; ///< no hardware flow control USART_Init(USART3, &USART_InitStructure); And enable PE interrupt, and then, send parity error data to this discovery board. So, parity error interrupt is occurred successfully, but after this parity error intterupt is occured continuously (I cannot clear the PE error bit). The USART intterrupt is below.void USART3_IRQHandler (void) __irq
{ char tmpRcv; /// PE Interrupt (PE flag is cleared when the flag is read) if (USART_GetFlagStatus(USART3, USART_FLAG_PE) == SET) { }/// RXNE interrupt
else if (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == SET) { ///receive data (and the RXNE flag is cleared) tmpRcv = USART_ReceiveData(USART3); ....}
It seems that the PE flag is not cleared when the flag is read. Please help to solve this problem. best regards. #uart #stm32 #discovery #usart2014-06-01 9:03 PM
Hello,
I modified the usart intterupt handler as below and it seems to work correct.void USART3_IRQHandler (void) __irq
{ char tmpRcv;/// RXNE interrupt
if (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == SET) { if (USART_GetFlagStatus(USART3, USART_FLAG_PE) != SET) { ///receive data and clear RXNE interrupt flag tmpRcv = USART_ReceiveData(USART3); } else { tmpRcv = USART_ReceiveData(USART3); USART_GetFlagStatus(USART3, USART_FLAG_PE); } } }Is this sequence is correct ?
And, I think this code is not simple, if there are other better code, please let me know.best regards.
2014-06-01 9:06 PM
The PE is NOT cleared by reading the status, but rather reading the data register.
2014-06-01 9:22 PM
#define USART_FLAG_ERRORS (USART_FLAG_ORE | USART_FLAG_NE | USART_FLAG_FE | USART_FLAG_PE)
void USART3_IRQHandler(void)
{
if (USART_GetFlagStatus(USART3, USART_FLAG_ERRORS) == SET)
{
USART_ReceiveData(USART3); // Discarded read to clear
}
/// RXNE interrupt
if (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == SET)
{
char tmpRcv;
///receive data (and the RXNE flag is cleared)
tmpRcv = USART_ReceiveData(USART3);
....
}
}