STM32F4 Cube HAL UART. Is it a bug or am I missing something?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-05 7:33 PM
I am using interrupt based UART IO (no DMA).
HAL_UART_Transmit_IT
function setsEIE
bit inCR3
register. According to STM32F407 datasheet (and real behaviour), this generates interrupt only in multi buffer mode (whenDMAR
bit is set).EIE
enables interrupt generation for frame error (FE
), overrun error (ORE
), noise error (NE
). This error, as I understand, only for receiving.Part of
HAL_UART_IRQHandler
function:tmp1 = __HAL_UART_GET_FLAG(huart, UART_FLAG_ORE);
tmp2 = __HAL_UART_GET_IT_SOURCE(huart, UART_IT_ERR); /* UART Over-Run interrupt occurred ----------------------------------------*/ if ((tmp1 != RESET) && (tmp2 != RESET)) { __HAL_UART_CLEAR_OREFLAG(huart);huart->ErrorCode |= HAL_UART_ERROR_ORE;
}if
(huart->ErrorCode != HAL_UART_ERROR_NONE) { /* Set the UART state ready to be able to start again the process */ huart->State = HAL_UART_STATE_READY;HAL_UART_ErrorCallback(huart);
}HAL_UART_IRQHandler
checks for each error. If error occurred andEIE
bit is set, it resets UART state, but doesn't reset interrupt enabling bits, soTXE
interrupt will be always generated, butUART_Transmit_IT
function treats stateHAL_UART_STATE_READY
as invalid and doesn't do anything. Infinite loop.Part of
UART_Transmit_IT
function:static
HAL_StatusTypeDef UART_Transmit_IT(UART_HandleTypeDef *huart) { uint16_t* tmp; uint32_t tmp1 = 0; tmp1 = huart->State; if ((tmp1 == HAL_UART_STATE_BUSY_TX) || (tmp1 == HAL_UART_STATE_BUSY_TX_RX)) { } else { return HAL_BUSY; } } Is it a bug in Cube HAL? #stm32 #stm32f4 #hal #hal #uart #usart #interrupts #bug #stm32f4- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-09 5:13 AM
Hi ns.rublag,
I understand the bug, it will be reported to development team.-Shahrzad-- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-16 6:38 PM
This BUG is also true for receiving data.
I have a BT module with a ''connected'' GPIO. So I enable the USART after this pin goes high. This takes some time and the PC does not know about it, so data is send as soon as the BT connection is established. This results in overrun errors and that triggers the bug... My workaround used the UART_Error_Callback function: void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart) { if (huart->ErrorCode == HAL_UART_ERROR_ORE){ // remove the error condition huart->ErrorCode = HAL_UART_ERROR_NONE; // set the correct state, so that the UART_RX_IT works correctly huart->State = HAL_UART_STATE_BUSY_RX; } } but a general solution is probably a lot more difficult ...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-25 7:42 AM
Hi all,
This bug is already known.,
Regarding error detection, maybe another thing that could be reminded: when errors are detected, state is updated in order to allow further API calls (not to remain blocked in some cases, with default (empty) error handling). In HAL_UART_IRQHandler(), Error flag is cleared in ICR register, and ErrorCode is updated to keep error type for user. Then, HAL_UART_ErrorCallback() is called. In HAL, this function is defined with “Weak� attribute, with an empty body. Error handling procedure has to be defined and implemented in a new HAL_UART_ErrorCallback() function, in user code, that will supersede weak one. -Shahrzad-- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-20 12:59 PM
Is there any update from ST about this? Will it be fixed in a future version of the HAL?