STM32F4 APB1 Prescaling Issue
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-04-19 1:54 AM
Posted on April 19, 2014 at 10:54
Hi all,
I'm curious about prescaling APB1 for the STM32F4. I'm building a triangle wave generator and frequency meter, for which it is conveniant for me to have a high as possible clock frequency for Timers 4 and 6. Therefore I've been playing with the APB1 prescaler (ie bits 12:10 of RCC_CFGR). I have a function adapted from the STM DAC output example which produces a triangle wave, using TIM6 as its clock base. I've got a function written so I can basically get any frequency in the range 1Hz to 166kHz. By default (according to mysystem_stm32f4xx.c
) the APB1 has a prescaler of 4 from a HCLK which I happen to know is running at 168MHz. When I change the APB1 prescaler to 2, my output frequency accordingly doubles. When I try to change it 1 however, it just prescales it to 2. Then I noticed the ref manual (RM0090) says you can't prescale the APB1 below 42MHz which kind of explains it, but doesnt explain why it manages to prescale the APB1 by a value of 2 when its initially 42MHz .Any thoughts about this, anyone with experience prescaling APB1? Thanks, Jonathan #stm32f4 #apb1 #prescaler
Labels:
- Labels:
-
RCC
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-04-19 4:18 AM
Posted on April 19, 2014 at 13:18
Read the manual carefully.
1. You should not set APB1clock to more than 42MHz. 2. If the prescaler is 1, the *timers'* clock is equal to APB clock; if the prescaler is 2 and more, the timers' clock is twice the APB clock. JW