2018-10-24 03:15 AM
HI
I NEED ENABLE BRUST MODE WITH COMPRATOR FOR CURRENT CONTROL WITH HARDWAER ON HRTIMER
AFTER CURRENT MORE THAN SETING IGNORE ONE SWICHING PERIOD
2018-10-24 04:28 AM
cool, sounds exciting...
now, can you translate that for us ?
F335 Phase shift hardware... 3 phase ? like power factor correction ? is that 50/60Hz ?
Enable Burst mode with comparitor .. ADC ? I guess..
I am lost... too much detail missing...
do you have a circuit diagram ?
are you following an example ?
what are you trying to achieve ?
2018-10-27 05:15 AM
STM32F334 HAVE HRTIMER FOR MAKE DC/DC ONLY ONE CHANEL CAN DRIVE MOSFET POSETIVE AND NEGATIVE BOUTH WHEN POSETIVE HIGH NEGATIVE LOW AND WHEN NEGATIVE HIGH POSETIVE LOW I NEED SOME TIME POSETIVE AND NEGATIVE BOUTH PUT TO LOW ONLY WITH BRUST MODE CAN DO THIS
HOW IS POSSIBLE COMPRATOR INSIDE IC CONNECT FOR ENABLE BRUST MODE
2018-10-27 05:54 AM
please draw a diagram, I cannot guess what you need.