cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F334 PHASE SHIFT HARDWARE CURRENT CONTROL

omid hamdi
Senior

HI

I NEED ENABLE BRUST MODE WITH COMPRATOR FOR CURRENT CONTROL WITH HARDWAER ON HRTIMER

AFTER CURRENT MORE THAN SETING IGNORE ONE SWICHING PERIOD

3 REPLIES 3
T J
Lead

cool, sounds exciting...

now, can you translate that for us ?

F335 Phase shift hardware... 3 phase ? like power factor correction ? is that 50/60Hz ?

Enable Burst mode with comparitor .. ADC ? I guess..

I am lost... too much detail missing...

do you have a circuit diagram ?

are you following an example ?

what are you trying to achieve ?

omid hamdi
Senior

STM32F334 HAVE HRTIMER FOR MAKE DC/DC ONLY ONE CHANEL CAN DRIVE MOSFET POSETIVE AND NEGATIVE BOUTH WHEN POSETIVE HIGH NEGATIVE LOW AND WHEN NEGATIVE HIGH POSETIVE LOW I NEED SOME TIME POSETIVE AND NEGATIVE BOUTH PUT TO LOW ONLY WITH BRUST MODE CAN DO THIS

HOW IS POSSIBLE COMPRATOR INSIDE IC CONNECT FOR ENABLE BRUST MODE

T J
Lead

please draw a diagram, I cannot guess what you need.