2014-03-06 5:40 AM
Hi
,I would like to
know
if is possible set
a timer
or other peripheral on the STM32F30x
to count
up or down
the pulses applied
to a pin
depending on the
logic level
applied
to a second
input
. For example if the second input is high the pulse are counted Up instead if the second input is low the pulse are counted Down.I have carefully read
the
timersection on the
reference manual
but have not found
how to set
the timer
to achieve this functionality
.Please let me know. Thank you.
#stm32f30x2014-03-21 10:07 AM
#1 I apply the clock at PA.6 configured as alternate function 2. Then the CCMR1 is configured for IC1-TI1. When I toggle the clock signal I see change the bit6 in PA IDR register so no hardware connection error happen. In this condition and with SMS=001 the count change (increment o decrement) instead RM0090 say ''Counter counts up/down on TI2FP2 edge''.
#2 the problem is not spurious count at startup but the counting direction that depend of the initial level of the clock signal.Why
does it happen?
How do I
know
the internal state
?
This is may Main code and register value at runtime.int main(){
// FLASH->ACR // // SystemCoreClock variable: Contains the core clock (HCLK) = 72MHz // // HSE = 8MHz // SYSCLK = 72MHz // HCLK = 72MHz // AHB = 72MHz // APB1 = 36MHz // APB2 = 72MHz // CLOCK enable RCC->AHBENR |= RCC_AHBENR_GPIOAEN + // GPIOA clock 0; RCC->APB1ENR |= RCC_APB1ENR_TIM3EN + // TIM3 clock 0; RCC->APB2ENR |= 0 + // 0; //-------------------------------------------------- PORTA GPIOA->MODER |= GPIO_MODER_MODER1_0 + // PA.1 Out GPIO_MODER_MODER6_1+GPIO_MODER_MODER7_1+ // PA.6, PA.7 alternate Function Mode 0; GPIOA->AFR[0] = (2UL<<28)+(2UL<<24); // PA.6, PA.7 alternate Function 2 GPIOA->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR0 + // PA.0 High Speed GPIO_OSPEEDER_OSPEEDR1 + // PA.1 High Speed GPIO_OSPEEDER_OSPEEDR6 + GPIO_OSPEEDER_OSPEEDR7 + // PA.6, PA.7 High Speed 0; GPIOA->PUPDR |= 0; //-------------------------------------------------- TIM3 TIM3->CR1 = TIM_CR1_CKD_1/*+TIM_CR1_CKD_0*/; // Clk digital filter 36MHz/4 TIM3->CR2 = 0; TIM3->CCMR1 = (TIM_CCMR1_IC1F_0+TIM_CCMR1_IC1F_1+TIM_CCMR1_IC1F_2+TIM_CCMR1_IC1F_3) + // Filter 36MHz/4/32/8=35KHz(28us) TIM_CCMR1_CC2S_0+TIM_CCMR1_CC1S_0; // IC2-TI2, IC1-TI1 TIM3->CCMR2 = 0; TIM3->CCER = 0; TIM3->PSC = 1; TIM3->ARR = 0x100; //TIM3->SMCR = 0; //TIM3->EGR = TIM_EGR_UG; TIM3->SMCR = /*TIM_SMCR_SMS_3+TIM_SMCR_SMS_2+TIM_SMCR_SMS_1*/+TIM_SMCR_SMS_0+ //0001: Encoder mode 1 0; TIM3->CR1 |= TIM_CR1_CEN; //TIM3->EGR = TIM_EGR_UG; while(1){ int32_t k; for (k=1000; k>0; k--) ; SpareCounter32++; GPIOA->ODR ^= GPIO_ODR_1; } }2014-03-21 11:03 AM
#2 the problem is not spurious count at startup but the counting direction that depend of the initial level of the clock signal.
Why
does it happen?
How do I
know
the internal state
? I don't know, it's not how the functionality is described. The documentation for the TIM units is not particularly good, and the block diagrams lack detail. I'd prefer to see some more gate-level stuff, it would be less ambiguous. These TIM operations are somewhat outside my purview.