User Activity

Posted on April 08, 2015 at 13:09I'm trying to use the CRC peripheral on STM32F3 to calculate the CRC at byte-level but I can not get the same result as indicated in application note AN4187. The following snippet of code should return a CRC equal to...
Posted on March 06, 2014 at 14:40Hi, I would like to know if is possible set a timer or other peripheral on the STM32F30x to count up or down the pulses applied to a pin depending on the logic level applied to a second input. For example if the se...