STM32F303VC DAC signal generation and period measure using EXTI interrupt
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-12 8:36 AM
Posted on May 12, 2018 at 17:36
I'm trying to generate a square wave signal using the DAC channel 2 (PA5) with a 1.627 ms period and then measuring that by catching the rising edge trigger in an EXTI4 interrupt on the PF4 pin. The problem is that I have to use the DAC channel 1 to see the EXTI4 triggers and the measured period is not what I expect to be.
This is the complete program, I'm working using IAR Embedded Workbench 8.22:&sharpinclude 'header.h'
&sharpinclude <math.h> &sharpinclude <stdio.h> &sharpdefine N 100 //&sharpdefine tau 1.38*pow(10,-8) int j=0, flag=0; float periodi[N]; void setup(){ RCC->AHBENR |= RCC_AHBENR_GPIOAEN | RCC_AHBENR_GPIOFEN; RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN; RCC->APB1ENR |= RCC_APB1ENR_TIM2EN | RCC_APB1ENR_TIM3EN | RCC_APB1ENR_DACEN; GPIOA->MODER |= GPIO_MODER_MODER5; GPIOF->MODER |= GPIO_MODER_MODER4; NVIC->ISER[0] |= (1<<10 | 1<<29); SYSCFG->EXTICR[2] |= SYSCFG_EXTIRCR_EXTI4_PF; EXTI->IMR |= EXTI_IMR_MR4; EXTI->RTSR |= EXTI_RTSR_TR4; } void setupTIM2(){ TIM2->PSC = 71; TIM2->CR1 |= TIM_CR1_CEN; TIM2->CNT = 0; } // 65536 : 0.0009*PSC = 65536 : 0.8135 ==> PSC = 0.8135 / 0.0009 ==> PSC = 904 // 65536 : 0.8228 = ARR : 0.8135 ==> ARR = (65536 / 0.8228) * 0.8135 = 64795 void setupTIM3(){ TIM3->PSC = 903; TIM3->ARR = 64795; TIM3->DIER |= TIM_DIER_UIE; TIM3->CR1 |= TIM_CR1_CEN; TIM3->CNT = 0; } void TIM3_IRQHandler(){ TIM3->SR &= ~TIM_SR_UIF; //printf('TIM3\n'); if(flag==0){ DAC->DHR12R1 = 0; flag = 1; for(int i=0; i<1000; i++); } else{ DAC->DHR12R1 = 4095; flag = 0; for(int i=0; i<1000; i++); } } void EXTI4_IRQHandler(){ EXTI->PR |= EXTI_PR_PR4; //printf('EXTI4\n'); if(j<N){ periodi[j] = TIM2->CNT*tau; j++; TIM2->CNT = 0; } else{ TIM2->CR1 &= ~TIM_CR1_CEN; TIM3->CR1 &= ~TIM_CR1_CEN; DAC->CR &= ~DAC_CR_EN1; } } void setupDAC(){ DAC->CR |= DAC_CR_EN1; } void main(){ setup(); setupDAC(); setupTIM2(); setupTIM3(); while(1); }#exti-handler #interrupt #dac #stm32f3 #embedded-softwares
Labels:
- Labels:
-
DAC
-
GPIO-EXTI
-
Interrupt
-
STM32F3 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0