cancel
Showing results for 
Search instead for 
Did you mean: 

RTC Interrupt not accurate when place a function in

jd kim
Associate II
Posted on May 12, 2018 at 15:32

I just used RTC interrupt to measure msec timing. and  I got some problem.

when i write naive code in interrupt there is no problem. timing is correct and no delay. the sample code is below

void RTC_IRQHandler(void)

{

   val = RTC->CNTL ;

   dif = val - ex;

   msec++;

   if (msec >= 1000)

   {

   sec++;

   msec = 0;

   }

   ex = RTC->CNTL ;

}

 but when i use a function to replace with the code the timing have delay almost half

void RTC_IRQHandler(void)

{

   val = RTC->CNTL ;

   dif = val - ex;

   timing(); // just same with previous code.

ex = RTC->CNTL ;

}

void timing()

{

   msec_++;

   

if (msec_ >= 1000)

   {

   sec_++;

   msec_ = 0;

   }

}

to clarify, i write the two code in same time. but change nothing

void RTC_IRQHandler(void)

{

   val = RTC->CNTL ;

   dif = val - ex;

   msec++;

   if (msec >= 1000)

   {

   sec++;

   msec = 0;

   }

   

timing(); // the timing is same and also has same delay

   ex = RTC->CNTL ;

}

wtf? I didn't change any clock config. why this interrupt is not occur in correct timing when i use any simple function?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0