2021-07-20 2:22 AM
using stm32f303re to write data in the st M95160w EEPROM and reading back the written data. the problem is i am not getting back the accurate output.
the output should be like this:
status 0x02
11 22 33
status 0x00
but getting
status 0x02
00 ff ff
status 0x00
Here is the Code:
#include "main.h"
#include <stdio.h>
SPI_HandleTypeDef hspi1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
const uint8_t EEPROM_READ = 0b00000011; //Read from Memory Array
const uint8_t EEPROM_WRITE = 0b00000010; //Write to Memory Array
const uint8_t EEPROM_WRDI = 0b00000100; //Write Disable
const uint8_t EEPROM_WREN = 0b00000110; //Write Enable
const uint8_t EEPROM_RDSR = 0b00000101; //Read Status Register
const uint8_t EEPROM_WRSR = 0b00000001; //Write Status Register
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_SPI1_Init(void);
int main(void)
{
char uart_buf[50];
int uart_buf_len;
char spi_buf[20];
uint8_t addr;
uint8_t wip;
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_SPI1_Init();
// CS pin should default high
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Say something
uart_buf_len = sprintf(uart_buf, "SPI Test\r\n");
HAL_UART_Transmit(&huart2, (uint8_t *)uart_buf, uart_buf_len, 100);
// Enable write enable latch (allow write operations)
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_WREN, 1, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Read status register
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_RDSR, 1, 100);
HAL_SPI_Receive(&hspi1, (uint8_t *)spi_buf, 1, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Print out status register
uart_buf_len = sprintf(uart_buf,"Status: 0x%02x\r\n",(unsigned int)spi_buf[0]);
HAL_UART_Transmit(&huart2, (uint8_t *)uart_buf, uart_buf_len, 100);
// Test bytes to write to EEPROM
spi_buf[0] = 0x11;
spi_buf[1] = 0x22;
spi_buf[2] = 0x33;
// Set starting address
addr = 0x01;
// Write 3 bytes starting at a given address
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_WRITE, 1, 100);
HAL_SPI_Transmit(&hspi1, (uint8_t *)& addr, 1, 100);
HAL_SPI_Transmit(&hspi1, (uint8_t *)spi_buf, 3, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Clear buffer
spi_buf[0] = 0;
spi_buf[1] = 0;
spi_buf[2] = 0;
// Wait until WIP bit is cleared
wip = 1;
while (wip)
{
// Read status register
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_RDSR, 1, 100);
HAL_SPI_Receive(&hspi1, (uint8_t *)spi_buf, 1, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Mask out WIP bit
wip = spi_buf[0] & 0b00000001;
}
// Read the 3 bytes back
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_READ, 1, 100);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&addr, 1, 100);
HAL_SPI_Receive(&hspi1, (uint8_t *)spi_buf, 3, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Print out bytes read
uart_buf_len = sprintf(uart_buf,"0x%02x 0x%02x 0x%02x\r\n",(unsigned int)spi_buf[0],(unsigned int)spi_buf[1],(unsigned int)spi_buf[2]);
HAL_UART_Transmit(&huart2, (uint8_t *)uart_buf, uart_buf_len, 100);
// Read status register
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&EEPROM_RDSR, 1, 100);
HAL_SPI_Receive(&hspi1, (uint8_t *)spi_buf, 1, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
// Print out status register
uart_buf_len = sprintf(uart_buf,"Status: 0x%02x\r\n",(unsigned int)spi_buf[0]);
HAL_UART_Transmit(&huart2, (uint8_t *)uart_buf, uart_buf_len, 100);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
}
static void MX_SPI1_Init(void)
{
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}