STM32F29 PWM with Timer 2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-08 10:47 AM
In my code for pwm on timer 2 in stm32F429, I have to use multiple channels (2 at a time). However only my channel 1 pin is giving pwm output. Please advise me what to do
void enable_gpio1()//setting pin 5 of port a for AF1 which corresponds to timer 2.
{ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; //Enables port A input output pins by setting the corresponding bit in advanced high performance bus 1 register. GPIOA ->MODER |= GPIO_MODER_MODER5_1; //Configures pin 5 for alternate function mode by setting the corresponding bit in the mode register GPIOA ->OTYPER &= ~(GPIO_OTYPER_OT_5); //Makes the output type as push-pull by resetting the corresponding bit in output type register. GPIOA ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR5_1;//Makes the output high speed. GPIOA ->PUPDR &= ~(GPIO_PUPDR_PUPDR5);//No pull up or pull down. GPIOA ->AFR[0] = GPIO_AF1_TIM2<<20;//Sets the AF1 bit in the AFRL(AFR[0]) register which links AF1 to pin A5 }void enable_gpio2()//setting pin 2 of port a for AF1 which corresponds to timer 2.{ RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; //Enables port A input output pins by setting the corresponding bit in advanced high performance bus 1 register. GPIOA ->MODER |= GPIO_MODER_MODER2_1; //Configures pin 5 for alternate function mode by setting the corresponding bit in the mode register GPIOA ->OTYPER &= ~(GPIO_OTYPER_OT_2); //Makes the output type as push-pull by resetting the corresponding bit in output type register. GPIOA ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR2_1;//Makes the output high speed. GPIOA ->PUPDR &= ~(GPIO_PUPDR_PUPDR2);//No pull up or pull down. GPIOA ->AFR[0] = GPIO_AF1_TIM2<<20;//Sets the AF1 bit in the AFRL(AFR[0]) register which links AF1 to pin A5 }void generate_pwm1(int n){ TIM2 ->CCMR1 |= TIM_CCMR1_OC1M_2; TIM2 ->CCMR1 |= TIM_CCMR1_OC1M_1; TIM2 ->CCMR1 &= ~(TIM_CCMR1_OC1M_0);//Selects pwm mode 1 by writing 110 TIM2 ->CCMR1 |= TIM_CCMR1_OC1PE;// TIM2 ->CR1 |= TIM_CR1_ARPE;//Enables preload register TIM2 ->EGR |= TIM_EGR_UG;//Enables update event whenever cnt equals ccr. TIM2 ->CCER |= TIM_CCER_CC1P;//Sets the polarity of the pwm TIM2 ->CCER |= TIM_CCER_CC1E; TIM2 ->ARR = (int)n*40/250.0;//Sets the value for the auto reload register. TIM2 ->CCR1 = 1;//Sets the value for the ccr register. TIM2 ->CR1 |= TIM_CR1_CEN;//Starts the counter for timer 2.}void generate_pwm2(int n){ TIM2 ->CCMR2 |= TIM_CCMR2_OC3M_2; TIM2 ->CCMR2 |= TIM_CCMR2_OC3M_1; TIM2 ->CCMR2 &= ~(TIM_CCMR2_OC3M_0);//Selects pwm mode 1 by writing 110 TIM2 ->CCMR2 |= TIM_CCMR2_OC3PE;// TIM2 ->CR1 |= TIM_CR1_ARPE;//Enables preload register TIM2 ->EGR |= TIM_EGR_UG;//Enables update event whenever cnt equals ccr. TIM2 ->CCER |= TIM_CCER_CC3P;//Sets the polarity of the pwm TIM2 ->CCER |= TIM_CCER_CC3E; TIM2 ->ARR = (int)n*40/250.0;//Sets the value for the auto reload register. TIM2 ->CCR3 = 1;//Sets the value for the ccr register. TIM2 ->CR1 |= TIM_CR1_CEN;//Starts the counter for timer 2.}My channel 1 pwm is working but channel 3 is not. I have also included the code I have used to enable the gpio pins.
#timer2 #stm32 #pwmSolved! Go to Solution.
- Labels:
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-09 9:48 AM
Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-09 12:45 PM
Hello again!!
The correct answer about your posted code , belongs to
Waclawek.Jan
‌ and toTurvey.Clive.002
‌
- « Previous
-
- 1
- 2
- Next »