cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f207 LCD

ezrab
Associate II
Posted on August 08, 2011 at 10:13

hi.

 i would like to start anew project with stm32f207 with lcd.

i know that the stm32f207 can controll lcd throw FSMC bus my question is whats the maximum size of lcd i can use and how do find whitch LCD monitors i can connect to FSMC?

thanks very much for your help.
10 REPLIES 10
Posted on August 08, 2011 at 17:44

The size limit of the LCD's that attach directly with a DMA type interface, is the availability of enough memory to act as a video buffer.

For large displays you're going need to look for panels with build in controllers, and video memory.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ezrab
Associate II
Posted on August 15, 2011 at 14:01

what are my options i am looking for avery cheep lcd and as big as possiable .

how do i know what size will work?

and what kind of LCD can i connect to the FSMC BUS?

thanks.

Posted on August 15, 2011 at 21:36

Physical size or resolution?

You are going to have to provide some bounding conditions on pricing and size. Where's you're min/max sweet point?

What's considered cheap for a 42'' panel is probably a lot different than for one that's 2'', 3'' or 4''.

 

See what people are using on STM32 dev boards, plenty of vendors on eBay, and at least one guy who comes to this forum once a month hawking his wares. See what displays ST is using, get part# and find a vendor to quote equivalent displays.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ezrab
Associate II
Posted on August 16, 2011 at 07:09

hi.

i am looking for somthing between 4'''' to 7'''' max.

st is using asmall one 3'''' i am looking for somthing bigger, and thats why i wanted to know is it possiable to connect 7'''' display lcd directly throw the FSMC bus?

if not what is the max one ?

price range 15-20$.

who is this guy? what is his name?

thanks alot.

rosarium
Associate II
Posted on August 16, 2011 at 10:34

I tried a 5.7'' TFT glass( without inbuilt controller) QVGA(320 x 240) resolution with STM32F2. It's working fine.

The thing which matters is the resolution. You can also drive a 7'' TFT of QVGA resolution by STM32F2.

ezrab
Associate II
Posted on August 16, 2011 at 11:40

thanks for the repaly.

 do you have the schamtic?

did you connect it throw the FSMC?

what king of LCD did you connected?

where can i find it?

thanks.

rosarium
Associate II
Posted on August 16, 2011 at 12:44

Yes the interface is FSMC. The schematic is under development. I tested the prototype using STM32F2 eval board.

The TFT is controller less. It is from ampire. the part no. is AM320240N6T MQWT50H-A(5.7'') .

ezrab
Associate II
Posted on August 16, 2011 at 15:52

hi.

where did you found that display i tried to find it on goolge but i didnt found nothing.

do you know the price?

thanks.

Posted on August 16, 2011 at 15:57

who is this guy? what is his name?

Jacky Sheng, he posts here every month, at least once, shouldn't have to scroll through more than a couple of pages to find one or more of this posts. I can't speak to his company, pricing or performance, but he's persistent and understands marketing.

Here a post from the second page, which appear to be particularly on point

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/3.5, 4.3 and 7 TFT with Touch LCD Controller provided!&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%]3.5, 4.3 and 7 TFT with Touch LCD Controller provided!

Also, for more information about Kitronix Display's products, please visit the following website:

http://kitronixdisplay.en.ecplaza.net/

Jacky Sheng

Kitronix Display (H.K.) Limited

Tel:

+86-189-2939-0669

E-mail:

mailto:jacky_sheng@126.com

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..