2020-05-07 7:19 AM
Hello,
I am using UART4 from a STM32F2. I am sending a data then my RXNE FLAG from SR register go from 0 to 1. Without doing anything (no read of the DR register and no clearing manually the flag) it go back to 0 after some time. So I am missing the data in my IT routine.
I can't figure out why this happening. Could someone have an idea of what the issue could be ?
2020-05-07 8:15 AM
>RXNE should be set when you *receive* data, not when *sending* it from the STM32 USART.
Yeah sure. I am sending a data then the flag is set when I received it.
> How do you know?
Knowing that I'm doing nothing on DR ? or knowing that the flag is going to 0 ? for the second case I am knowing it by checking the SR register
2020-05-07 8:21 AM
>>RXNE should be set when you *receive* data, not when *sending* it from the STM32 USART.
> Yeah sure. I am sending a data then the flag is set when I received it.
So you have some loopback enabled?
> for the second case I am knowing it by checking the SR register
Okay so post a minimal but complete compilable code exhibiting the problem.
JW
2020-05-07 8:32 AM
>So you have some loopback enabled?
Yes hardware one my TX is going on my RX pins
> Okay so post a minimal but complete compilable code exhibiting the problem.
Ok I will clean the code to send you the minimal one I used (The application is huge and old) I will clear all the thing I comment and send it.
Thanks for your help !
2020-05-20 8:57 AM
Here is the code simplified :
main :
int main(void)
{
DISABLE_INTERRUPTS();
/* Setup STM32 system tickclock, AFIO clocks (alternate function dedicated clock */
RCC_init();
UART_Init();
ENABLE_INTERRUPTS();
FLAG_IT_UART4 = 0x40004C00;
FLAG_IT_EN_UART4 = 0x40004C0C;
USART_SendData(UART4, 0x0A);
while(1);
return(0); //pour traiter warning compilo
}
RCC_init
void RCC_init(void)
{
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB |
RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD |
RCC_AHB1Periph_GPIOE, ENABLE);
/* Enable SYSCFG's APB interface clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
if (SysTick_Config(SystemCoreClock / 100000)) //DORIAN_MPLX passage de 1000 à 100000 pour 10 us
{
/* Capture Error */
while(1);
}
}
Uart_init
void UART_Init(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4); /* pour UART4 en PC10, PC11 */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
/* Configure the GPIO ports( USARTx Transmit and Receive Lines) */
/* Configure the USARTx_Tx as Alternate function Push-Pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Enable USARTx clocks */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
// Clear structure to default values
USART_DeInit(USART1);
USART_DeInit(USART2);
USART_DeInit(USART3);
USART_DeInit(UART4);
USART_DeInit(UART5);
/*-- UART MPLX configured as follow:------------------------
- Word Length = 8 Bits
- 1 Stop Bit
- No parity
- BaudRate = 9600 baud
- Receive and transmit enabled
-------------------------------------------------------*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No ;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART4, &USART_InitStructure);//WARNING NOT POSSIBLE
// no USART_ClockInit(), car valeurs par defaut(reset) sont OK, DG 24/03/2011 15:25:48
//UART MPLX Enable Interrupt
//DORIAN_MPLX ETAPE 1 prio originel : 6
NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 6;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_Init(&NVIC_InitStructure);
USART_ITConfig(UART4, USART_IT_RXNE, ENABLE);
USART_ITConfig(UART4, USART_IT_TC, ENABLE);
USART_Cmd(UART4, ENABLE);
}
UART4_IRQHandler:
void UART4_IRQHandler(void)
{
static u8 u8_Data1;
if(USART_GetITStatus(UART4, USART_IT_RXNE) != RESET)
{
u8_Data1 = (USART_ReceiveData(UART4) & 0xFF);
}
if(USART_GetITStatus(UART4, USART_IT_TC) != RESET)
{
USART_ClearITPendingBit(UART4, USART_IT_TC);
}
}
2020-05-20 8:58 AM
I put my brake point on the first if before calling receive
2020-05-20 10:01 AM
And, in the debugger, when the breakpoint is hit, you watch the USART registers?
JW
2020-05-22 12:13 AM
I am watching the 2 pointer :
First for the SR register
Second for CR1 to be sure everything is well activated
2020-05-27 6:06 AM
I read all the documentation and don't find answer to this behaviour.
Have you any idea or where to search ?
2020-05-27 8:07 AM
What toolchain are you using that " FLAG_IT_UART4 = 0x40004C00 " is a pointer?
Don't breakpoint the code.
Don't inspect the USART registers in the debugger.
Read the register SR, and reflect content to a pin or pins, perhaps in SysTick. Perhaps watch for transitions in main() loop and print. Avoid prints in interrupts, or where byte-time critical.
Consider if your handler is reentering due to something debugger (not specified) is doing.
The SR won't auto-clear, you're touching DR/SR somewhere.
Make something absolutely minimal, where you have no interaction for a) other code, b) debugger side access of the SAME hardware registers.
2020-06-08 8:14 AM
Hi Clive,
Thank you for your answer.
yes, FLAG_IT_UART4 is a pointer to an u32.
I follow your advice and apparently it's the monitoring of the SR register through the debugger which reset the flag. Now I don't understand why and I'm asking if you know what could be a reason to this behaviour ? something to configure in the debugger itself ?
Breakpoint doesn't affect the state of the flag.