STM32F2 RXNE flag FROM SR register clear without reason
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-07 7:19 AM
Hello,
I am using UART4 from a STM32F2. I am sending a data then my RXNE FLAG from SR register go from 0 to 1. Without doing anything (no read of the DR register and no clearing manually the flag) it go back to 0 after some time. So I am missing the data in my IT routine.
I can't figure out why this happening. Could someone have an idea of what the issue could be ?
- Labels:
-
STM32F2 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-07 8:15 AM
>RXNE should be set when you *receive* data, not when *sending* it from the STM32 USART.
Yeah sure. I am sending a data then the flag is set when I received it.
> How do you know?
Knowing that I'm doing nothing on DR ? or knowing that the flag is going to 0 ? for the second case I am knowing it by checking the SR register
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-07 8:21 AM
>>RXNE should be set when you *receive* data, not when *sending* it from the STM32 USART.
> Yeah sure. I am sending a data then the flag is set when I received it.
So you have some loopback enabled?
> for the second case I am knowing it by checking the SR register
Okay so post a minimal but complete compilable code exhibiting the problem.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-07 8:32 AM
>So you have some loopback enabled?
Yes hardware one my TX is going on my RX pins
> Okay so post a minimal but complete compilable code exhibiting the problem.
Ok I will clean the code to send you the minimal one I used (The application is huge and old) I will clear all the thing I comment and send it.
Thanks for your help !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-20 8:57 AM
Here is the code simplified :
main :
int main(void)
{
DISABLE_INTERRUPTS();
/* Setup STM32 system tickclock, AFIO clocks (alternate function dedicated clock */
RCC_init();
UART_Init();
ENABLE_INTERRUPTS();
FLAG_IT_UART4 = 0x40004C00;
FLAG_IT_EN_UART4 = 0x40004C0C;
USART_SendData(UART4, 0x0A);
while(1);
return(0); //pour traiter warning compilo
}RCC_init
void RCC_init(void)
{
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB |
RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD |
RCC_AHB1Periph_GPIOE, ENABLE);
/* Enable SYSCFG's APB interface clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
if (SysTick_Config(SystemCoreClock / 100000)) //DORIAN_MPLX passage de 1000 Ã 100000 pour 10 us
{
/* Capture Error */
while(1);
}
}Uart_init
void UART_Init(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4); /* pour UART4 en PC10, PC11 */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
/* Configure the GPIO ports( USARTx Transmit and Receive Lines) */
/* Configure the USARTx_Tx as Alternate function Push-Pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Enable USARTx clocks */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
// Clear structure to default values
USART_DeInit(USART1);
USART_DeInit(USART2);
USART_DeInit(USART3);
USART_DeInit(UART4);
USART_DeInit(UART5);
/*-- UART MPLX configured as follow:------------------------
- Word Length = 8 Bits
- 1 Stop Bit
- No parity
- BaudRate = 9600 baud
- Receive and transmit enabled
-------------------------------------------------------*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No ;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART4, &USART_InitStructure);//WARNING NOT POSSIBLE
// no USART_ClockInit(), car valeurs par defaut(reset) sont OK, DG 24/03/2011 15:25:48
//UART MPLX Enable Interrupt
//DORIAN_MPLX ETAPE 1 prio originel : 6
NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 6;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_Init(&NVIC_InitStructure);
USART_ITConfig(UART4, USART_IT_RXNE, ENABLE);
USART_ITConfig(UART4, USART_IT_TC, ENABLE);
USART_Cmd(UART4, ENABLE);
}UART4_IRQHandler:
void UART4_IRQHandler(void)
{
static u8 u8_Data1;
if(USART_GetITStatus(UART4, USART_IT_RXNE) != RESET)
{
u8_Data1 = (USART_ReceiveData(UART4) & 0xFF);
}
if(USART_GetITStatus(UART4, USART_IT_TC) != RESET)
{
USART_ClearITPendingBit(UART4, USART_IT_TC);
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-20 8:58 AM
I put my brake point on the first if before calling receive
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-20 10:01 AM
And, in the debugger, when the breakpoint is hit, you watch the USART registers?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-22 12:13 AM
I am watching the 2 pointer :
- FLAG_IT_UART4 = 0x40004C00;
- FLAG_IT_EN_UART4 = 0x40004C0C;
First for the SR register
Second for CR1 to be sure everything is well activated
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-27 6:06 AM
I read all the documentation and don't find answer to this behaviour.
Have you any idea or where to search ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-27 8:07 AM
What toolchain are you using that " FLAG_IT_UART4 = 0x40004C00 " is a pointer?
Don't breakpoint the code.
Don't inspect the USART registers in the debugger.
Read the register SR, and reflect content to a pin or pins, perhaps in SysTick. Perhaps watch for transitions in main() loop and print. Avoid prints in interrupts, or where byte-time critical.
Consider if your handler is reentering due to something debugger (not specified) is doing.
The SR won't auto-clear, you're touching DR/SR somewhere.
Make something absolutely minimal, where you have no interaction for a) other code, b) debugger side access of the SAME hardware registers.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-08 8:14 AM
Hi Clive,
Thank you for your answer.
yes, FLAG_IT_UART4 is a pointer to an u32.
I follow your advice and apparently it's the monitoring of the SR register through the debugger which reset the flag. Now I don't understand why and I'm asking if you know what could be a reason to this behaviour ? something to configure in the debugger itself ?
Breakpoint doesn't affect the state of the flag.
- « Previous
-
- 1
- 2
- Next »