cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103x8 pin compatible or LQFP48 alternative

lk.dgironi
Associate III

Hi all,

I've a board with the STM32F103C8T6 MCU.

My firmware has to handle a lot of IO, display and UART logic, nothing special but just a lot of logic.

So the 64K b internal flash memory is almost full.

I've a couple of question here:

1) can i switch to the STM32F103CBT6 so that I'll have 128Kb of flash without issues?

2) Is there any other candidate in a small package (like the LQFP-48) I can use? I have to use a small package cause I don't have that much space available on that board (find attached)

 

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions

 As I said previously, no issue to migrate directly to 128kB!

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

The answer is provided in the datasheet:

SofLit_1-1730718861807.png

SofLit_2-1730718919938.png

The only difference is the Flash size so you don't have to worry.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks, so it's a yes on my request "1)", no issues replacing with STM32F103CBT6.

dsCapture.PNG

 As I said previously, no issue to migrate directly to 128kB!

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
lk.dgironi
Associate III

Thanks!