STM32F103VET6 Multiple DMA giving incorrect data.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-20 10:35 PM - edited 2024-10-20 10:36 PM
I have an STM32F103VET6 with multiple DMA Channels like UART2_RX, ADC, UART3_RX, UART3_TX, all at different priorities. The first one or two bytes of every DMA Channel becomes incorrect all of a sudden in runtime and corrects back only after power restart. Has anyone else also faced this issue? I have previously used multiple DMAs without any trouble in STM32F4 MCUs. Is it the change to Cortex-M3 that is causing trouble? I am thinking to implement a mutex (virtually, without RTOS) to restrict the DMA to one stream at a time. Is there any better solution?
Labels:
- Labels:
-
ADC
-
DMA
-
STM32F1 Series
-
UART-USART
0 REPLIES 0