2024-10-20 9:39 PM
In our application we are using part no STM32G0KCIU6 of LQFP32 / UFQFPN32 - GP package.in application we are using USB communication there by we also required 16Mhz HSE, but in this package Pin No 2 of MCU has additional options to configure as OSC_IN whether this pin can be configured for HSE requirement?
2024-10-20 10:17 PM
Hello @Jin2 and welcome to the ST Community.
The pin that you mentioned can be used as an oscillator input pin for HSE Oscillator. You can't use a HSE Crystal since you will need two pins (OSC_IN. and OSC_OUT). Refer to the step 4 of this article: https://community.st.com/t5/stm32-mcus/how-to-use-stm32cubemx-to-configure-hse-high-speed-external/ta-p/49604 to understand the difference between them.
As a conclusion : you can have a HSE on this pin (an oscillator and not a cristal one).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-20 10:23 PM
Thanks!!
Can I use 48Mhz xtal oscillator? It is our requirement. can be possible to tie on 2nd pin of the controller?
Can be possible to use the same or similar this MPN?
https://www.digikey.com/en/products/detail/ecs-inc/ECS-3225MV-480-BN-TR/9646074
2024-10-20 11:37 PM
I suggest you to take a look at this discussion. It should be really helpful. Also, the only pin that can be used is the OSC_IN we already mentionned.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.