2024-10-03 11:17 PM - edited 2024-10-03 11:36 PM
hi
i used of CRC in stm32CubeMX and for check true worked CRC used of two online CRC calculator site:
https://www.sunshine2k.de/coding/javascript/crc/crc_js.html
&
https://crccalc.com/?crc=123456789&method=&datatype=0&outtype=0
i think stm32cubeIDE internal CRC use of standard CRC32_MPEG2:
Polynomial = 0x4C11DB7
Initial value = 0xFFFFFFFF
Final XoR Value = 0x0
Input reflected = disable
Result reflected = disable
Am I correct and have I written the CRC parameter values for stm32f103 exactly right?
...........
but CRC result for stm32CubeIDE different with online CRC calculator site?
example:
stm32 CRC for 0x00 = 0xc704dd7b
online CRC calculator site for 0x00 = 0x4E08BFB4
stm32 CRC for 0x01 = 0xc3c5c0cc
online CRC calculator site for 0x01 = 0x4AC9A203
stm32 CRC for 0x02 = 0xce86e615
online CRC calculator site for 0x02 = 0x478A84DA
stm32 CRC for 0xFF = 0x76f39dcf
online CRC calculator site for 0xFF = 0xFFFFFF00
............ my Code:
#include "main.h"
void SystemClock_Config(void);
int main(void)
{
extern CRC_HandleTypeDef hcrc;
//CRC
uint32_t buff[2];
uint32_t result = 0xffffffff;
uint32_t i = 0;
//
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_I2C1_Init();
MX_SPI1_Init();
MX_CRC_Init();
while (1)
{
i = 0;
while(i < 256)
{
buff[0] = i;
result = HAL_CRC_Calculate(&hcrc, &buff[0], 1);
i++;
}
}
}
-------------------------
please help me
Solved! Go to Solution.
2024-10-04 12:26 AM
The CRC unit in 'F1 calculates CRC only from 32-bit words, so for example for your 0x01 input it uses 0x00000001 (big endian, so 0x00 0x00 0x00 0x01):
JW
2024-10-03 11:27 PM - edited 2024-10-03 11:34 PM
Hi,
Are you using the polynomial reversed, or the reciprocal?
Kind regards
Pedro
2024-10-03 11:44 PM
stm32cubeIDE CRC for STM32F103RE is constant value and can not change any CRC parameter.
and i used for one Byte value.
0
1
2
0xFF
I don't make any changes to the data.
I have read various CRC documents from st company and nowhere I have seen the value of CRC parameters used for STM32F103 so I don't know if it uses Reverse or Reciprocal or not.
2024-10-04 12:06 AM
Hi,
The CRC unit needs to be Reset between each set of calculations. If HAL doesn't have a reset function, then try something like -
CRC->CR |= CRC_CR_RESET;
before i = 0;
I hope this helps.
Kind regards
Pedro
2024-10-04 12:26 AM
The CRC unit in 'F1 calculates CRC only from 32-bit words, so for example for your 0x01 input it uses 0x00000001 (big endian, so 0x00 0x00 0x00 0x01):
JW
2024-10-04 12:37 AM
HAL automatic reset for function "HAL_CRC_Calculate()"
2024-10-04 1:53 AM
thanks thanks thanks