cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 FreeRTOS problem

Adam Klekotko
Associate
Posted on April 19, 2018 at 18:13

The original post was too long to process during our migration. Please click on the attachment to read the original post.
1 REPLY 1
Pavel A.
Evangelist III
Posted on April 19, 2018 at 23:51

It looks like the target or debugger settings are incorrect (or the problem is in the debugger start script) and the debugger cannot connect. From the information provided, it's hard to tell more.

-- pa