2017-07-20 8:37 AM
Hello everyone,
I'm trying to make this code works :
/*♯♯-1- Link the micro SD disk I/O driver ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
if(FATFS_LinkDriver(&SD_Driver, SDPath) == 0) { /*♯♯-2- Register the file system object to the FatFs module ♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if(f_mount(&SDFatFs, (TCHAR const*)SDPath, 0) != FR_OK) { /* FatFs Initialization Error */ Error_Handler(); } else { /*♯♯-3- Create a FAT file system (format) on the logical drive ♯♯♯♯♯♯♯♯♯*/ /* WARNING: Formatting the uSD card will delete all content on the device */ if(f_mkfs((TCHAR const*)SDPath, 0, 0) != FR_OK) { /* FatFs Format Error */ Error_Handler(); }}
}
The fm_mkfs function gets out at that line in the ff.c file of the FatFs library:
if (disk_write(pdrv, tbl, b_vol, 1)) /* Write it to the VBR sector */
return FR_DISK_ERR;To be precise it gets out in the SD_WriteMultiBlocks (custom disk_write function) function :
SD_Error SD_WriteMultiBlocks(const uint8_t *writebuff, uint64_t WriteAddr, uint16_t BlockSize, uint32_t NumberOfBlocks)
{ SD_Error errorstatus = SD_OK;TransferError = SD_OK;
TransferEnd = 0; StopCondition = 1; SDIO->DCTRL = 0x0;SDIO_ITConfig(SDIO_IT_DCRCFAIL | SDIO_IT_DTIMEOUT | SDIO_IT_DATAEND | /*SDIO_IT_RXOVERR*/SDIO_IT_TXUNDERR | SDIO_IT_STBITERR, ENABLE);
SD_LowLevel_DMA_TxConfig((uint32_t *)writebuff, (NumberOfBlocks * BlockSize)); SDIO_DMACmd(ENABLE);if (CardType == SDIO_HIGH_CAPACITY_SD_CARD)
{ BlockSize = 512; WriteAddr /= 512; }/* Set Block Size for Card */
SDIO_CmdInitStructure.SDIO_Argument = (uint32_t) BlockSize; SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SET_BLOCKLEN; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure);errorstatus = CmdResp1Error(SD_CMD_SET_BLOCKLEN);
if (SD_OK != errorstatus)
{ return(errorstatus); }..... /* Other commands in the function...*/
......
}
It returns : SD_CMD_RSP_TIMEOUT.
I can't figure out why all the previous commands worked but this one (which also worked on previous calls).
Any clue will be appreciated.
Thank you.
Mathias
#fatfs-sdio #stm32f1032018-08-08 6:50 AM
Bumping to remove from the home page (No Answer Posts)
Writes might fail in ST's assorted models if code hasn't waited for prior read/write operations to have completed properly. Check IRQHandlers and callbacks