Skip to main content
Explorer
June 28, 2024
Question

FatFs f_open() hard fault

int main(void)
{
FATFS FatFs;

FIL fil;

FRESULT fr;

UINT bw;

 

fr = f_mount(&FatFs, "", 0);

if (fr != FR_OK) {

return (int)fr;

}

fr = f_open(&fil, "example.txt", FA_WRITE | FA_CREATE_ALWAYS);

if (fr != FR_OK) {

 

f_mount(NULL, "", 0);

return (int)fr;

}

f_close(&fil);

}
This is the main.c file. While running the code I get a hard fault issue at f_open. 

I use SDIO mode SD 1 bit

Kindly help

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
June 28, 2024

Whatever is happening, it's not in this top-level code. No idea of STM32 or board involved.

Establish where the hard fault is actually occurring. Do this with a suitably instrumented HardFault_Handler() rather than a while(1) loop

Would suggest moving FATFS structure off the stack, and clearing the other structures.

Returning from main() will fail and potentially fault the MCU, where would it return too?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AScha.3
Super User
June 28, 2024

First you have to mount - successful ! -> check return , ok or not.

And do mount with "1" parameter, = now. 

And WHAT you mount ? an empty string ??

see :

fresult = f_mount(&SDfs, (TCHAR const*)SDPath, 1);			// SD card mount NOW

Then only if fresult = ok , can do any open or read ; NOT write, until this working fine !!!

If you feel a post has answered your question, please click on " Best Answer ".