2015-03-28 9:59 AM
Hello.
I try enable TIM12-17 but TIM12EN-TIM17EN not set to 1 (always 0) in APB1ENR and APB2ENR.?an you help me?Thanks. #stm32f100rc2015-10-29 1:41 AM
Hello,
Has this ever been fixed or answered? I'm facing the same problem with an STM32F100RC that I have here. I'm unable to use TIMER 12 (even enabling TIM12EN in RCC_APB1ENR isn't working).Kind regards.2015-10-29 3:10 AM
2015-10-29 3:49 AM
Sorry I don't have any access to that link. Can you resend a valid one?
Thanks in advance2015-10-29 6:48 AM
Hi logie.jurgen,
The other discussion is . As I said there, please check the used revision of STM32F100 device. To do it, read the exact value of ''DEV_ID'' field in DBGMCU_IDCODE register (0xE0042000): - If the value is 0x420 or 0x428, refer to RM0041 - Otherwise, refer to RM0 -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.