cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32F0 I2C comunication trouble

stanislav
Associate
Posted on October 29, 2015 at 15:02

What is wrong here?

I try to read 2 bytes data of temperature sensor LM73 by I2C of STM32F0Discovery based on STM32F051 micro. The micro is waiting RXNE event and doesn't exit from the loop.

I don't see any activity on SDA and SCL lines The signals have the pullup resistors.

Here is a code bellow:

void init_I2C1(void) {

  

I2C_InitTypeDef I2C1_InitStructure;       // I2C1 Configuration structure

 /** I2C1 GPIO Configuration  

  PB6   ------> I2C1_SCL

  PB7   ------> I2C1_SDA

  */

  /*Enable or disable the AHB peripheral clock */

  RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

  

/* IC1 Configuration */

 // I2C_Cmd(I2C1,DISABLE);

  

  /*Configure GPIO pin : PB */

  GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7;

  GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;

  GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;  

  GPIO_Init(GPIOB, &GPIO_InitStruct);

  

  I2C1_InitStructure.I2C_Mode  = I2C_Mode_I2C;

  /*Timing register value is computed with the AN4235 xls file,

   fast Mode @400kHz with I2CCLK = 48MHz, rise time = 140ns, fall time = 40ns */

  I2C1_InitStructure.I2C_Timing = 0x00B01A4B;// 400KHz | 8MHz-0x00310309; 16MHz-0x10320309; 48MHz-50330309  I2C1_InitStructure.I2C_OwnAddress1 =0;

  I2C1_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C1_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;

  I2C1_InitStructure.I2C_DigitalFilter = 0x00;

  I2C1_InitStructure.I2C_OwnAddress1 = 0x00;

  I2C1_InitStructure.I2C_Ack = I2C_Ack_Enable;  

  I2C1_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;  

  I2C_Init(I2C1, &I2C1_InitStructure);

  

  I2C_MasterRequestConfig(I2C1,I2C_Direction_Receiver); // Master reading mode   

  I2C1->CR1 |= I2C_IT_RXI;    // Enable RXNE Event

//  GPIO_SetBits(GPIOB,GPIO_Pin_8);// Power up 

  Delay(10);

  I2C_Cmd(I2C1,ENABLE);

/*Read function*/

void I2C1MasterBufferRead() {

   

I2C_TransferHandling(I2C1,(LM73_BASE_ADDR),2,I2C_AutoEnd_Mode,I2C_Generate_Start_Read);

    while(I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE) == RESET);

    ucI2CReadBuff[0] = I2C_ReceiveData(I2C1);

    while(I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE) == RESET);    

    ucI2CReadBuff[1] = I2C_ReceiveData(I2C1);

    while(I2C_GetFlagStatus(I2C1, I2C_ISR_STOPF) == SET);

    I2C_ClearFlag(I2C1,I2C_FLAG_STOPF); 

 }

 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0