2015-12-21 2:58 AM
Hi,
From what I read in the datasheets I suspect that I can run the timers at 48MHz. Is there a way to let the timers (a timer) run with 96MHz? I stumbled across that when I played around with Cube. Best regards, Christian.2015-12-21 3:08 AM
Of course not, this is just incompet^H^H^H^H^H^H^H^Hmistake of CubeMX makers.
To quote from RM0091 Rev.8, both Fig11 and and Fig12 for the timer clock say: ??????????????????? ?????????????? which in turn is a buggy PDF creator used to generate the datasheet. Rewriting this manually: If (APB1 prescaler = 1) x1 else x2. IMO this is clear enough. JW2015-12-21 3:50 AM
...just what I thought. Thanks.