cancel
Showing results for 
Search instead for 
Did you mean: 

HAL ticks and timer rollover

mda2376
Associate II
Posted on June 04, 2014 at 14:57

The HAL_GetTick() is used implement timeouts within the HAL library with code similar to:

      /* Get timeout */

      timeout = HAL_GetTick() + HSE_TIMEOUT_VALUE;

      

      /* Wait till HSE is disabled */  

      while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) != RESET)

      {

        if(HAL_GetTick() >= timeout)

        {

          return HAL_TIMEOUT;

        }      

      }

However there is no consideration for timer rollover which will occur after approximately 47 days. This will lead to unexpected behavior where a timeout will fire before the timeout period expires. Unfortunately similar timer code to this is used pervasively throughout the HAL.

On a related note is there an official bug tracker for the HAL library, or is this forum the suggested route for reporting bugs?

Matt

#i-want-to-smack-people
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on June 04, 2014 at 16:13

Is the clock/interrupt even ticking at this point?

The new library is full of this amateurish crap...

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/%5bbug%20report%5d%20Bug%20in%20HAL%20%28SPL%29%20delay%20function&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=230]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2F[bug%20report]%20Bug%20in%20HAL%20%28SPL%29%20delay%20function&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=230

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32F4xx%20HAL_TIM_IRQHandler%20misses%20interrupts%20on%20nearly%20overlapping%20TIM%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=73]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fSTM32F4xx%20HAL_TIM_IRQHandler%20misses%20interrupts%20on%20nearly%20overlapping%20TIM%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Java%2FAllItems.aspx¤tviews=73

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32CubeF4%20__HAL_UART_CLEAR_FLAG%20macro%20is%20incorrect&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=58]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fSTM32CubeF4%20__HAL_UART_CLEAR_FLAG%20macro%20is%20incorrect&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Java%2FAllItems.aspx¤tviews=58
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mda2376
Associate II
Posted on June 04, 2014 at 16:52

SysTick may not be active at this point - I simply copied the first example of this timeout structure I saw. There are about 150 places throughout the HAL with this defect.

So the developer must assume that any call that can return HAL_TIMEOUT may return HAL_TIMEOUT at random even when there is no underlying failure.. I suppose this is marginally better than the library becoming stuck in a tight loop polling for a bit that will never become set.

Thanks for the link, I see ST is already aware of this problem.

Posted on June 17, 2014 at 17:29

Hi Matt,

We have already the limitation in the STM32Cube HAL bugs list, it is resolved within CubeL0, and will be fixed in next releases of CubeF4 (early July).

Thanks for the report.

With regards.

jorg
Associate
Posted on December 21, 2015 at 13:13

My bad, please forget about my previous post.

I re-checked and I suppose there should not be any tick overrun problem with the HAL I use.

Sorry for the spam.