2019-12-05 1:42 AM
Hi there,
currently I am trying to set up the CAN peripheral on the STM32F042K6 and it is getting stuck while initializing the according GPIOs. The CPU gets stuck at the HAL_GPIO_Init line, I am not able to connect with an ST Link without connecting under hardware reset and the system is not going into the Error_Handler.
GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_CAN;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
While the GPIO_PIN_11 is the CAN RX pin and can be initialized flawlessly. GPIO_PIN_12 is the CAN TX pin and it is not working. I have not experienced something like this while working with any STM32 product.
Here some infos about my code gernation:
Code generated with CubeMX 5.4.0
Firmware package used: F0_V1.11.0
I really hope there is someone able to help me.
Best whishes
Tristan
2019-12-05 2:37 AM
> The CPU gets stuck at the HAL_GPIO_Init line,
Make sure there's no hardware issue with the pin - shorts, or a connected device which potentially shorts the power supply momentarily.
JW
PS. Change your username to a normal nick.