2017-08-23 8:47 AM
Hi,
I am having trouble getting some basic USART up and running on the STM32F0308-DISCO board. I have tried both sending and receiving and don't seem to see anything coming through on either end. My code is as follows:
Thanks in advance.
#include 'stm32f0xx.h'
#include 'string.h' #define BSRR_VAL 0x0300 void usart_init( void );/*-----------------------------------------------------------------------------*/
void usart_init( void ) { USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure;RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOB, ENABLE );
RCC_APB2PeriphClockCmd( RCC_APB2Periph_USART1, ENABLE );/* Configure USART2 pins */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init( GPIOB, &GPIO_InitStructure ); GPIO_PinAFConfig( GPIOB, GPIO_PinSource8, GPIO_AF_1 ); GPIO_PinAFConfig( GPIOB, GPIO_PinSource9, GPIO_AF_1 );/* Config USART */
USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init( USART1, &USART_InitStructure );USART_Cmd( USART1, ENABLE );
}/*-----------------------------------------------------------------------------*/
void output_init( void )
{ RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOC, ENABLE );GPIO_InitTypeDef GPIO_InitStructure;
GPIO_StructInit( &GPIO_InitStructure ); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init( GPIOC, &GPIO_InitStructure ); } /*-----------------------------------------------------------------------------*/int main(void)
{output_init();
usart_init(); while (1) { //usart_send_str( 'moving to 180' ); //while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); //USART_SendData( USART1, (uint8_t)'X' ); while ( USART_GetFlagStatus( USART1, USART_FLAG_RXNE) == RESET );char ch = (char)USART_ReceiveData( USART1 );
if ( ch == 'o' ) GPIOC->BSRR = BSRR_VAL; else if ( ch == 'f' ) GPIOC->BRR = BSRR_VAL; } } #stm32f0 #usart Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-08-23 10:44 AM
PB8 and PB9 are USART pins?
2017-08-23 12:48 PM
I had been playing around with several pins, those must have been the most recent I tried. I also tried PA2 and PA3 with no success.
2017-08-23 12:55 PM
2017-08-23 3:15 PM
PA2 and PA3 should at least have some connectivity to a USART peripheral, and a free for use on the board.
2017-08-24 6:09 AM
OK, so since my device is an STM32F030R8 device, I should be using USART2 with PA2 and PA3, is this correct?
I have just tried this and I am still not seeing anything.
2017-08-24 6:26 AM
According to the table from the DS I posted above, there's no USART connectivity on PA2 and PA3 for STM32F030x8.
JW
2017-08-24 6:49 AM
Hi to everyone!
Checking the user's manual of the discovery board there shows that the pins that you are using to uart are free, pages 19 and 20:
By the way, the right pins are PA9 and PA10, there you havean issue.
I have a question, how are you testing that the uart is not working? are you plugging the board to the computer through a usb-to-serial converter and checking in a terminal if data is received? I made a test code for a nucleo board F030 using CubeMX and System Workbench, and as the nucleoSTLink chips works also as usb-to-serial brigde, for making the test is fast, here is the post:
https://community.st.com/thread/40685-stm32-cubemx-uart?commentID=156868#comment-156868
As the Discovery STlink chip doesn't works as usb-to-serial bridge you should use one external. I recommend to you to use CubeMX for initialize the peripherals, there you can be ''sure'' about the pins that are available in your board.
2017-08-24 7:10 AM
According to the document provided by
Turvey.Clive.002
, there should be ( see below ). Or am I misunderstanding?I have also tried using USART1 and PA9 and PA10, which should work according to the table below, but I have had no luck.
2017-08-24 7:40 AM
I apparently have an older version of DS missing the footnote 3...
Then USART2 on PA2/3 should work.
As Clive said, make sure the pins are free on that board. Check them as GPIO Input/Output.
What's written on the chip and what is its ID readout?
JW