cancel
Showing results for 
Search instead for 
Did you mean: 

SPI slave bidirectional

chris wedgwood
Associate
Posted on August 25, 2017 at 12:09

I have a difficulty with ST32F030 and Slave SPI

I'm trying to have it respond to an spi command:-

Master sends 0x05, slave responds with an array of 7 bytes.

It kind of works the first time, but then loses sync, and get OVR bit set. I can't figure out why.

Heres the code:-

int main(void)

{

   HAL_Init();

   /* Configure the system clock */

   SystemClock_Config();

   /* Initialize all configured peripherals */

   MX_SPI1_Init();

   spi_init();

   while (1)

   {

      HAL_SPI_Receive_IT(&hspi1, &spiData[0], 1);

   }

}

/* SPI1 init function */

static void MX_SPI1_Init(void)

{

   hspi1.Instance = SPI1;

   hspi1.Init.Mode = SPI_MODE_SLAVE;

   hspi1.Init.Direction = SPI_DIRECTION_2LINES;

   hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

   hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

   hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

   hspi1.Init.NSS = SPI_NSS_SOFT;

   hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

   hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

   hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

   hspi1.Init.CRCPolynomial = 7;

   hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

   hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

   /* SPi priority interrupt configuration */

   HAL_NVIC_SetPriority(SPI1_IRQn, 1, 1);

   if (HAL_SPI_Init(&hspi1) != HAL_OK)

   {

      Error_Handler();

   }

}

void SPI1_IRQHandler(void)

{

   HAL_SPI_IRQHandler(&hspi1);

}

uint8_t spiData[8];

uint8_t edgesmsg[7];

void spi_interrupt()

{

   uint8_t c;

   c = spiData[0];

   if ( c == 0x05)

      HAL_SPI_Transmit(&hspi1, edgesmsg, 7, 1000);

}

Any suggestions gratefully received..

#spi #slave
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0