2024-04-19 01:50 AM
I have a STM32F405RGT6 on a custom PCB and are using a ST-Link/V2 ISOL in my computer. A USB-Mini is conencted to the ST-Link and from the ST-Link I use RESET, SWCLK, SWIO and GND to my STM32.
I have tried connecting to the ST-Link with the STM32CubeProgrammer with the following settings:
Port: SWD
Frequency: 4000
Mode: Normal
Access port: 0
Reset Mode: Software reset
Speed: Reliable
Shared: Disabled
Debug in Low Power mode: ON
Before connecting I have updated the driver to the latest according to the STM32CubeProgrammer:
Version: V2J43S7
After updating the driver I tried to connecting to the MCU and recieve the same error every time:
Error: No STM32 target found! If your product embeds Debug Authenication, please perfrom a discovery using Debug Authentication
(I have also tried with different settings and it gave the same error)
I have tried following steps on the following guide:
https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693
In the steps I have followed all the steps until 3.2 where I cant debug the main.c file in the Src folder.
I receive this error when trying to debug:
I have chosen the .elf file in the Debug folder as shown here:
How do I manually enter the offset for the ELF file in the lanch configuration or disable symbol loading for the ELF file?
If there is another way to solve the "Error: No STM32 target found! If your product embeds Debug Authenication, please perfrom a discovery using Debug Authentication" error I am all ears.
Thank you.
Solved! Go to Solution.
2024-04-19 03:30 AM
I noticed a wiring issue with the not having a common ground to the ST-link and then got 3.79V as the target voltage. Once I had the target voltage at 3.79V I could connect! Thank you Andrew for your help. Really appreciate it.
2024-04-19 02:02 AM
see:
So your target has no power - or you didnt connect to st-link VDD input ; st-link "see" no target with power.
2024-04-19 02:19 AM
@mathieusteketee wrote:A USB-Mini is conencted to the ST-Link and from the ST-Link I use RESET, SWCLK, SWIO and GND to my STM32.
Words are a particularly poor way to describe electrical connections - that's why we have schematics (aka "circuit diagrams")
As @AScha.3 said, you also need a VDD reference to the ST-Link.
2024-04-19 02:20 AM
Hi AScha.3, thank you for your quick reply.
Might be the target does not have power. I have not connected the ST-link VDD input since the MCU recieves 3.3V from the PCB. Is it necessary to set 3.3V on the VDD pin?
2024-04-19 02:25 AM - edited 2024-04-19 02:31 AM
@mathieusteketee wrote:I have not connected the ST-link VDD input since the MCU recieves 3.3V from the PCB.
The purpose of the ST-Link's VAPP connection is not to supply power to the target, but for the ST-Link to detect that the target is powered. It's how the ST-Link knows that there's a Target connected.
It is also used as the reference for the ST-Link's voltage translators.
When the ST-Link does not detect power from the Target, it assumes that there is no Target present.
EDIT:
From the ST-Link User Manual:
2024-04-19 02:31 AM
My applogies, here you go:
2024-04-19 02:34 AM
I see, thank you for your reply Andrew! 😁
I will try to set power on the VDD then.
2024-04-19 02:35 AM
Note that VAPP is the input on the ST-Link.
2024-04-19 03:18 AM
I have tried setting 3.3V to the VAPP, Pin 1, (also tried pin 2) and recieved 2.84VDC at the target voltage:
But it seems when I refresh it jumps to 1.39VDC. Is this normale?
However I still get the error (with 2.84VDC):
2024-04-19 03:30 AM
I noticed a wiring issue with the not having a common ground to the ST-link and then got 3.79V as the target voltage. Once I had the target voltage at 3.79V I could connect! Thank you Andrew for your help. Really appreciate it.