cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX MDK-ARMV5 project generation problem

blaz2
Associate
Posted on April 08, 2015 at 14:50

Hi,

I have a problem with MDK-ARMV5 project generation if the project is located on a network drive. Everything else is generated.

If I have the project on a local disk everything works OK. 

I know that this is a simple solution but we keep all the data on network drives that are backed up regularly.

Does anyone else experience such problems?

Thanks 
3 REPLIES 3
Amel NASRI
ST Employee
Posted on April 08, 2015 at 19:25

What kind of problems are you facing? Is it at generation level or when compiling project?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

blaz2
Associate
Posted on April 10, 2015 at 10:28

It is at generation level.When I click Generate source code in Cube MX it generates source code (Drivers, Inc, Middlewares and Src) but not the project folder (MDK-ARM).

stm32cube-t
Senior III
Posted on April 16, 2015 at 14:30

Hello,

We don't reproduce your issue. Can you please provide the two log files from your <user>/.stm32cubemx directory?

Thank you