2018-04-24 2:07 AM
Hi,
I am trying to install STMCube on my mac, but the installation seems to fail.
I am using the following command from terminal:
sudo open SetupSTM32CubeMX-4.25.0.app
It fails with:
LSOpenURLsWithRole() failed with error -10810 for the file .../en.stm32cubemx/SetupSTM32CubeMX-4.25.0.app.
I also tried to open it with doubleclick, this doesn't work as well, the Cube symbol opens in the dock very briefly and then disappears..
Anyone else has the same issue?
Thanks
Till
2018-04-26 1:39 PM
I have this problem with MacOS X 10.13.4 (High Sierra). I have tried both the Java 8 and 10 64bit JDK and neither work.
It seems that the Mac installer is broken but you can get it to work by using the installer from the windows version on the command line as follows.
sudo java -jar SetupSTM32CubeMX-4.25.0.exe
Don't worry, the install script still detects that it is a Mac and installs OK.
It may have something to do with the installer wanting to write to
'/usr/share/applications'
and this is not possible due to the System Integrity Protection (SIP) introduced with MacOS X El Capitan.2018-05-11 4:53 AM
Next problem:
The integrated updater won't let me update.. Says i need to restart with administrator priviliges. Which i did, using sudo.
Still not working..
2018-08-02 7:58 AM
Still fails with 2.6.1
2018-08-02 2:16 PM
@Till Rachow, you installed as root, and installed in Applications. Don't do that. Install as regular user, and use a different directory. I use Developer.
to get the installer to install, you need to remove the quarantine flag since st doesn't sign their installers
xattr -d com.apple.quarantine <path to your installer>
2018-08-20 1:50 AM
@Mohamed Mansouri Please check @john doe 's answer. This stuff should be taken in to account for your installer, or should at least be somewhere in the manual..