STM32CubeMX 4.23.0 syscalls.c bugs ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-28 5:31 AM
Hi,
i'm using STM32CubeMX V 4.23.0 to build a project for a stm32f107vct with FatFs, LWIP & FreeRTOS using the gcc-arm-none-eabi-6-2017-q2-update toolchain.
Compiling the generated syscalls.c fails due various errors (see output below).
- One problem is that '
#
ifdef
_SYS_TIME_H_' should be '#
ifndef
_SYS_TIME_H_', because timezone is already defined via the generated <sys/time.h> include in gcc-arm-none-eabi-6-2017-q2-update/arm-none-eabi/include/sys/time.h and _SYS_TIME_H_ is therefore already set.#ifdef _SYS_TIME_H_
struct timezone {
int tz_minuteswest; /* minutes west of Greenwich */
int tz_dsttime; /* type of dst correction */
};
#endif
gcc relies on __asm_() instead asm() when using ANSI-C or STD-C so the following generated statement should be changed
caddr_t _sbrk(int incr)
{ extern char endasm
('end'); // should be__
asm__
('end'); static char *heap_end; char *prev_heap_end,*min_stack_ptr;
With best regards
Heiko Jakob
arm-none-eabi-gcc -mthumb -mcpu=cortex-m3 -mfloat-abi=soft -ffunction-sections -fdata-sections -Os -flto -fno-exceptions -Wall -DSTM32F107xC -c -g -Iinclude -Ilib/STM32CubeMX/Inc -Ilib/STM32CubeMX/Drivers/CMSIS/Include -Ilib/STM32CubeMX/Drivers/STM32F1xx_HAL_Driver/Inc -Ilib/STM32CubeMX/Drivers/CMSIS/Device/ST/STM32F1xx/Include -Ilib/STM32CubeMX/Middlewares/Third_Party/LwIP/src/include -Ilib/STM32CubeMX/Middlewares/Third_Party/LwIP/system -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/include -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM3 -Ilib/STM32CubeMX/Middlewares/Third_Party/FatFs/src -Ilib/STM32CubeMX/Middlewares/ST/STM32_USB_Device_Library/Core/Inc -std=c11 -MMD -MP -MF 'build/Debug/GNU_ARM_NONE_EABI_6_2017Q2-Linux/lib/STM32CubeMX/Src/syscalls.o.d' -o build/Debug/GNU_ARM_NONE_EABI_6_2017Q2-Linux/lib/STM32CubeMX/Src/syscalls.o lib/STM32CubeMX/Src/syscalls.c
lib/STM32CubeMX/Src/syscalls.c: In function '_sbrk':lib/STM32CubeMX/Src/syscalls.c:98:18: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'asm' extern char end asm('end'); ^~~lib/STM32CubeMX/Src/syscalls.c:98:18: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]lib/STM32CubeMX/Src/syscalls.c:103:15: error: 'end' undeclared (first use in this function) heap_end = &end; ^~~lib/STM32CubeMX/Src/syscalls.c:103:15: note: each undeclared identifier is reported only once for each function it appears inlib/STM32CubeMX/Src/syscalls.c: At top level:lib/STM32CubeMX/Src/syscalls.c:129:8: error: redefinition of 'struct timezone' struct timezone { ^~~~~~~~In file included from lib/STM32CubeMX/Src/syscalls.c:75:0:/opt/gcc-arm-none-eabi-6-2017-q2-update/arm-none-eabi/include/sys/time.h:50:8: note: originally defined here struct timezone { ^~~~~~~~- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-30 3:49 AM
Hello
jakob.heiko
,I confirm your reported issue and I raised it internally to the appropriate team.
Best Regards
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-30 8:59 AM
Hello
jakob.heiko
,I first thank you for your comment.
The timezone definition was necessary because of lwip:sockets.h. That code is coming from LWIP community and ST does not change it.
To avoid the timeval multidefinition, the pragma_SYS_TIME_H_ had to be defined at build level (btw: you should have it in the generated makefile), thus timezone had to be added 'manually', and this is done in the syscalls.c.
Have you modified the generated makefile ?
Kind regards
Sirma
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-04 4:45 AM
Hi
jakob.heiko
,Most recent available version of CubeMX I used, i.e. 4.25, brings new defines for compilation line in Makefile.
Please find here after some evidence log:
make -C Canada_MkI BINPATH=/cygdrive/c/gcc-arm/bin -f Makefile -k
make: Entering directory '/cygdrive/i/STM32/CUBE_MX/CubeMX_7921/support/Canada_MkI' mkdir build ... /cygdrive/c/gcc-arm/bin/arm-none-eabi-gcc -c -mcpu=cortex-m3 -mthumb -D_TIMEVAL_DEFINED -D_SYS_TIME_H_ -DUSE_HAL_DRIVER -DSTM32F107xC -DUSE_FULL_LL_DRIVER -I../Inc...
-Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF'build/ethip6.d' -MT'build/ethip6.d' -Wa,-a,-ad,-alms=build/ethip6.lst ../Middlewares/Third_Party/LwIP/src/core/ipv6/ethip6.c -o build/ethip6.o ... /cygdrive/c/gcc-arm/bin/arm-none-eabi-size build/Canada_MkI.elf text data bss dec hex filename 86072 500 41364 127936 1f3c0 build/Canada_MkI.elf /cygdrive/c/gcc-arm/bin/arm-none-eabi-objcopy -O ihex build/Canada_MkI.elf build/Canada_MkI.hex /cygdrive/c/gcc-arm/bin/arm-none-eabi-objcopy -O binary -S build/Canada_MkI.elf build/Canada_MkI.bin make: Leaving directory '/cygdrive/i/STM32/CUBE_MX/CubeMX_7921/support/Canada_MkI'NOTE: I modified the 'Project Settings', i.e.,in 'Advance Settings', 'Driver Selector' as LL for RTC.
Hope this helps completing this thread.
Regards.
Cyril