Skip to main content
GVita.11
Associate
December 16, 2020
Question

STM32CubeIDE example RTC smooth calibration for Nucleo F401RE?

  • December 16, 2020
  • 0 replies
  • 535 views

Dear community,

are new to STM32CubeIDE and ARM microcontrollers.

By reading the documentation available on the ST website, I was able to perform a large part of the application that I would like to create.

My project involves the construction of an acquirer with clock synchronized with GPS and PPS, sampling with high temporal precision.

Currently I was able to read the data from GPS,

started following the AN4759 guide for smooth calibration:

TIMER3 set so as to reset TIMER2 COUNTER every 32 PPS events (as suggested by the documentation on RTC AN4759). Unfortunately I can't take the next step. In other words, give TIMER2 the same clock as the RTC and then adjust the value in the calibration register.

How can I give the RTC clock to TIMER2?

Has anyone made something similar to take inspiration from for this board or microcontroller?

Any attempt made leads me to the same result, I get that the TIMER2 is connected to the system clock at 84MHz.

Greetings

Giuvi Giuva

This topic has been closed for replies.