cancel
Showing results for 
Search instead for 
Did you mean: 

STM32533RE - programming with nucleo ST-link

lectricidiot
Associate II

Hi,

Could someone be so kind as to explain in ***-proof terms exactly how I would connect an ST-link from a nucleo board to a custom STM32533RE PCB so that it can be programmed and debugged with STM32CubeIDE?  Which pins from the MCU do I need to make available on the PCB and how do they connect to the nucleo?  I haven't found a clear illustration of how to do this and some of the guides/comments I have seen have been conflicting!  I'm getting ready to send the PCB off to the fab house and want to make sure I've got this right as it would be an expensive mistake.

8 REPLIES 8
TDK
Super User

Connect SWDIO, SWCLK, GND at a minimum. Optionally connect NRST. Also optionally, connect TX/RX to take advantage of VCP functionality. Power must be supplied as well, generally does not come from the programmer.

> a nucleo board

Which one? They are not all the same. Some do not have programming capability without major modification. The user manual describes the pinouts if it has one.

If you feel a post has answered your question, please click "Accept as Solution".

Which NUCLEO? they make a few..

Generally you remove a pair of jumpers to disconnect the local target.

Connect SWDIO, SWCLK, NRST and GND from the debug header to your new board. For a standalone ST-LINK be able to connect its power to pin1 or 2 of the 20 pin ARM JTAG header to power the pods buffers.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi,

Thanks for the reply - I have NUCLEO-H743ZI2 and NUCLEO-H533RE boards available.  On closer inspection, it doesn't look like I can get access to the ST-LINK pins to program externally.  Can you recomend a nucleo or one of the standalone ST-LINKs?  I'm a little bit lost with which one I need to get.

Hi,

Thanks for the reply - I have NUCLEO-H743ZI2 and NUCLEO-H533RE boards available.  On closer inspection, it doesn't look like I can get access to the ST-LINK pins to program externally.  Can you recomend a nucleo or one of the standalone ST-LINKs?  I'm a little bit lost with which one I need to get!

I would get the STLINK-V3MINIE and use a standard programming header (FTSH-107-01-F-DV-K) to connect to the board.

STLINK-V3MINIE | Tool - STMicroelectronics

Pinout is detailed in the user manual.

If you feel a post has answered your question, please click "Accept as Solution".
mfgkw
Senior III

Most Nucleo-64 and Nucleo-144 boards with ST-Link/v2 older than H5* and H7* and N6* should work. At least all which can be broken to separate ST-Link from the target board.

Some of them are NUCLEO-64:

MB1136: NUCLEO-F030R8, NUCLEO-F070RB, NUCLEO-F072RB, NUCLEO-F091RC, NUCLEO-F103RB, NUCLEO-F302R8, NUCLEO-F303RE, NUCLEO-F334R8, NUCLEO-F401RE, NUCLEO-F410RB, NUCLEO-F411RE, NUCLEO-F446RE, NUCLEO-L010RB, NUCLEO-L053R8, NUCLEO-L073RZ, NUCLEO-L152RE , NUCLEO-L452RE, NUCLEO-L476RG, see UM1724

MB1319: NUCLEO-L412RB-P, NUCLEO-L433RC-P, NUCLEO-L452RE-P, see UM2206

MB1360: NUCLEO-G070RB, NUCLEO-G071RB, NUCLEO-G0B1RE, see UM2324

And some are NUCLEO-144:

MB1137: NUCLEO-F207ZG, NUCLEO-F303ZE, NUCLEO-F412ZG, NUCLEO-F413ZH, NUCLEO-F429ZI, NUCLEO-F439ZI, NUCLEO-F446ZE, NUCLEO-F722ZE, NUCLEO-F746ZG, NUCLEO-F756ZG,
NUCLEO-F767ZI, NUCLEO-H743ZI, see UM1974

MB1312: NUCLEO-L496ZG, NUCLEO-L496ZG-P, NUCLEO-L4A6ZG, NUCLEO-L4P5ZG, NUCLEO-L4R5ZI, NUCLEO-L4R5ZI-P, see UM2179

 

P.S.: some older Discovery boards will do the job as well with an internal ST-Link/v2. I found in my tray:

Discovery kit with STM32F407VG, see UM1472

Discovery kit with STM32L053C8, see UM1775

 

(or you follow Tesla's suggestion and buy an external ST-Link/v3.... I only have ST-Link/v2 up to now; they will work and are simpler and maybe they are cheaper. But /v3 will be faster at growing binary sizes...)

Brilliant, thank you for the help.  I will order one of those and design using that programming header.

 

Am I right in thinking that T_VCP_TX and T_VCP_RX connect to PA2 and PA3 (VCP_TX and VCP_RX respectively) on the STM32H5 so I can get VCOM?

Yes. T_VCP_TX is an input to the programmer, so connect it to (LP)U(S)ARTx_TX on the target mcu. Any UART can work, just needs to be configured correctly in your program.

If you feel a post has answered your question, please click "Accept as Solution".