cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C031C6 Timer confusion

MHank.1
Associate III

The code below links Timer1 in master mode to Timer3 in slave mode producing a 4 second toggle on PB8 and it works correctly.

My question is I'm not able to follow the flow of the signal in the Timer chart below the code.

If someone would show me the signal flow I would appreciate it. I have shown how I think the signal flows. Is this correct?

void LinkTimer1And3()

{

   // GPIOB clock enable

   RCC->IOPENR = 2;

   // Set PB8 alternate function

   GPIOB->MODER &= ~(3 << 16);

   GPIOB->MODER |= (2 << 16);

   // Alternate function to TIM3 CH1

   GPIOB->AFR[1] &= ~0x0f;

   GPIOB->AFR[1] |= 3;

   // Enable TIM1 and TIM3 clocks

   RCC->APBENR2 |= (1 << 11);

   RCC->APBENR1 |= (1 << 1);

   // Master Mode Selection - Select Update Event as Trigger output (TRG0)

   TIM1->CR2 |= (2 << 4);

   // Slave Mode Control Register - Configure in slave mode using ITR1 as

   //   internal trigger. External Clock Mode 1 - Rising edges of the selected

   //   trigger (TRGI) clock the counter.

   TIM3->SMCR |= 7;

   // Set Prescaler and Auto Reload Register to slow the

   //   processor down so we can see the LED blink.

   // Freq = 12MHz / ((12000 - 1) * (1000 - 1)) = 1Hz

   TIM1->PSC = 12000 - 1;

   TIM1->ARR = 1000 - 1;

   TIM3->PSC = 0;

   TIM3->ARR = 4 - 1;

   // OC1M Toggle output

   TIM3->CCMR1 |= (3 << 4);

   // CC1E Enable output

   TIM3->CCER |= 1;

   // Master Output Enable

   TIM3->BDTR |= (1 << 15);

   TIM1->CR1 |= 1;

   TIM3->CR1 |= 1;

   while(1);

}

0693W00000aHg2CQAS.png

PartsBin - An Electronic Parts Organizer for Windows @ JaxCoder.com
1 ACCEPTED SOLUTION

Accepted Solutions

0693W00000aHg6iQAC.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

Your Yellow line makes no sense. CK_INT comes from the RCC / APB clock sources, for the peripherals.

The other timer signal would come in via ITR, secondary clocking via ETR

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

0693W00000aHg6iQAC.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks, the more I looked at it the less sense it made but I couldn't find an alternative. Never thought to go to clock tree diagram.

That clears up a lot.

PartsBin - An Electronic Parts Organizer for Windows @ JaxCoder.com