2014-09-10 01:09 PM
Hi,
I have STM3210B and I am trying to connect it to PC. However, I am unable to connect it. I have installed all the STLink V2 drivers. Besides, I also download STVP tools as well, which installed its drivers.When I insert the usb in my PC, I do not get the new hardware found window. When I check in Device manager, I am unable to find the device connected. Please help me identify the problem, so I can fix it.Shashank2014-09-10 01:27 PM
The STM3210B-EVAL does NOT have an on-board ST-LINK, you are plugging in the boards USB connector, and it would need to be loaded with a USB firmware (VCP, MSC, etc) for your PC to recognize it.
2014-09-10 09:36 PM
2014-09-11 06:50 AM
So the ST-LINK is not getting detected? What version of Windows is this on? What version of the driver have you installed? Windows 8.x would required a signed driver, or system adjustments to accept an unsigned one.
Does the ST-LINK show up in Device Manager, what about in different USB ports, or different computers? If the ST-LINK is detected, then you should be able to plug into the STM3210B-EVAL via it's JTAG connector. Check the manual for the board if any special jumpering is required, I'd suspect not, but check. Use the ST-LINK Utilities to connect to the board, and confirm it can see the chip, and that it has current firmware on the ST-LINK.2014-09-12 09:45 AM
I am using Windows 7
I have installed drivers for STSW-STM3210STLINK does not gets detected in the device managerThe evaluation board does not has the firmware on the SD Card. Besides, I have installed the ST link utilities. However, it does not see the device at all.Besides, STLink does blink red in color when I plug it in. I am unable to understand what is the problem with the board.2014-09-12 10:01 AM
I have installed drivers for STSW-STM3210
What's that? The number is incomplete, can you provide a complete name and cite? This is what I'd think is appropriatehttp://www.st.com/web/en/catalog/tools/PF260218
I am unable to understand what is the problem with the board. You keep referring to the board, but the problem you have right now is getting the ST-LINK to work with your computer. Your inability to solve the first problem causes the secondary problem. If you continue to have problems with the ST-LINK perhaps you should inquire with the people you bought it from?2014-09-12 08:57 PM
Hello Clive.
I agree with what you had said. Yesterday, I spend all my time trying to deal with the STLINK V2 Driver. I think you have suggested the latest version of the stlink v2 driver, which I will try now. Let me check with it and I will get back to you. Thanks for the help.2014-09-12 08:59 PM
2014-09-13 06:26 AM
Hello Clive,
I just tried the driver you had suggested. However, still I am getting the same results. I have also checked the cable finally. But, I am getting the red blinking light. So, there is no problem with the cable. What do you think could else be the problem. Regards, Shashank2014-09-13 09:05 AM
If you see nothing in Device Manager (ST-Link or an !?) then you'll need to consider trying a different port, or computer. Does the cable work with other devices?