2014-09-10 1:09 PM
Hi,
I have STM3210B and I am trying to connect it to PC. However, I am unable to connect it. I have installed all the STLink V2 drivers. Besides, I also download STVP tools as well, which installed its drivers.When I insert the usb in my PC, I do not get the new hardware found window. When I check in Device manager, I am unable to find the device connected. Please help me identify the problem, so I can fix it.Shashank2014-09-14 4:26 AM
Hello Clive,
I tried connecting it to all the ports to my laptop. I even used an another laptop to try but nothing happened,. I could be a problem with the cable but I am not sure, because I get the status light on, blinking in red, on the stlink V2 device. It means that the power is applied to the device with the cable. I will try to use the cable with my digital camera and see if the cable is able to communicate the my laptop. I will let you know if it works.2014-09-19 6:47 AM
Hello Clive,
I got a new USB A to mini Cable of AWG 28 which is also used in blackberry mobile phones. I am able to successfully connect STLINK along with my STM3210B board. Thanks for all your help. Regards, Shashank Sayanwar.