cancel
Showing results for 
Search instead for 
Did you mean: 

SD Card detect pin initialization

matt-crc
Senior III

Hello,

Does anyone know how to link the sdcard_detect gpio pin in cubemx?  If the card is not inserted after power up, the system doesn't come up because  MX_SDMMC1_SD_Init(); fails.

I looked at: https://community.st.com/t5/stm32-mcus-embedded-software/understand-sd-card-detect-pin-initialization/td-p/758978

but I'm using AzRTOS, and I can't set the option in FatFS, and can't find the option in FileX.  

Can someone point me in the right direction?

thanks

Matthew

9 REPLIES 9
matt-crc
Senior III

Hi @mƎALLEm 

How do you link the SD_detect pin when AzRTOS is enabled?  it seems FATFS is grayed out in my CubeMX

mattcrc_0-1739932415607.png

I cant seem to find that option under FileX.

Thanks

Matthew

 

matt-crc
Senior III

I've added this code to prevent the system from crashing when initializing the SDMMC on powerup.

mattcrc_0-1739938840066.png

But is there an example somewhere on how to re-initialized the driver when a card is plugged in, and get AzRtos/FileX to start reading the SDMMC?  Is there anything in a library without having to re-write a basic function?

I looked at these examples, Fx_Dual_instance, and Fx_MultiAccess, but it seems it will only run if the card is plugged in, and i didn't find any code for the card detect pin.  Shouldn't that be part of the base Driver code?

Please see How To Insert Source Code - not as an image.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
matt-crc
Senior III

I've added this code to prevent the system from crashing when initializing the SDMMC on powerup.

static void MX_SDMMC1_SD_Init(void) {

	/* USER CODE BEGIN SDMMC1_Init 0 */
	if (HAL_GPIO_ReadPin(SD_Detect_GPIO_Port, SD_Detect_Pin) == 1) {
		printf("SD Card not found\r\n");
		return;
	} else {
		printf("SD Card Detected\r\n");
	}
	HAL_Delay(1000);
	/* USER CODE END SDMMC1_Init 0 */

 

But is there an example somewhere on how to re-initialized the driver when a card is plugged in, and get AzRtos/FileX to start reading the SDMMC?  Is there anything in a library without having to re-write a basic function?

I looked at these examples, Fx_Dual_instance, and Fx_MultiAccess, but it seems it will only run if the card is plugged in, and i didn't find any code for the card detect pin.  Shouldn't that be part of the base Driver code?

Hello @matt-crc 

Please refer to the example 'Projects/STM32U575I-EV/Applications/FileX/Fx_uSD_File_Edit' to manage card insertion/removal detection in your application.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
matt-crc
Senior III

Hi Omar @Saket_Om 

Correct me if I'm wrong, but it seems the software would go into ErrorHandler when main starts (line 247) if there is no card plugged in on bootup:

  if (HAL_SD_Init(&hsd1) != HAL_OK)
  {
    Error_Handler();
  }

So, if I can add code to check if card is present using:

    /* Check SD card detect pin */
    if (HAL_GPIO_ReadPin(SDCARD_DETECT_GPIO_Port, SDCARD_DETECT_Pin) == GPIO_PIN_SET)
    {
      ret = HAL_ERROR;
    }
    else
    {
      ret = HAL_OK;
    }

With the HAL_SD driver offline (card not inserted), the FX_thread does not start properly and will go into a while(1)

So, my questions are:

1- Do I need to re-initialize the HAL_SD driver each time a card is inserted?

2- what happens if a different size or type of card is inserted using your current demo, would the HAL driver need to be re-initialized anyway?

thanks

Matthew

 

 

Hello @matt-crc 

The code below is the initialization of the SDIO peripheral on the MCU. It is not related to the SD card.

  if (HAL_SD_Init(&hsd1) != HAL_OK)
  {
    Error_Handler();
  }

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
matt-crc
Senior III

Hi @Saket_Om 

HAL_SD_Init() calls HAL_SD_InitCard() which is supposed to get the parameters from the card.  So HAL_SD_Init() is related to the SD card.   

Hello @matt-crc 

You are right!

In this case, you can perform a check to detect the presence of the card before calling the HAL_SD_Init() function.

In the application mentioned above the card should plugged before running the code. Please see the readme.

Saket_Om_0-1740042625183.png

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om