2019-11-18 12:33 PM
Hi,
Just purchased a STM32072B-EVAL board and loaded an example project on it. I cleared it from memory using ST visual programmer and now the LCD display is blank (i use to see the GUI). Did i accidentally erase the GUI? If so can I download it back.
Thanks.
2019-11-18 12:44 PM
>>Did i accidentally erase the GUI?
You erased the original application replacing it with your own, thus removing it.
Perhaps should have saved original binary via STM32 Cube Programmer first.
Should be an Applications directory under the CubeF0 repository for the STM32072B-EVAL board, not sure if this would be an exact copy, or not.
Also should be other examples capable of driving the display
2019-11-18 12:49 PM
It contains the binary; it's SPL-based, though.
JW
2019-11-18 12:57 PM
Got it thx!