2021-01-03 3:20 AM
hi i have a problem with my uart program the thing is i have to determine the buffer size of the rx i'll call it rx_buff now i have multiple reception well different messages sizes some times 50bytes some times 2bytes but the problem is that when sending the 2 bytes the call back doesnt trigger until the full 50bytes are full until the rx_buff is full meaning i have to send the 2bytes message 25 times to get a callback is there a way to receive unknown messages with different length ?
using the stm32H750
thanks in advance
2021-01-03 3:59 AM
If you can guarantee there will be a pause after your 2-byte short message, then you could consider using the "Receiver timeout interrupt" present in the USARTs/UARTs. No I don't know how to do that from ST's software layers; I access the registers directly.
What I tend to do is arrange a DMA-driven circular receive-buffer, and then poll that.
Hope this helps,
Danish
2022-09-22 12:13 AM
No DMA:
Have a buffer with size bigger than your incoming data may be. After init, enable UART RX Timeout by:
HAL_UART_ReceiverTimeout_Config(&huart1,35);// for me, 35=37ms for baud9600
HAL_UART_EnableReceiverTimeout(&huart1);
Then insert your UART ERROR callback and include inside it the RTO:
void HAL_UART_ErrorCallback(UART_HandleTypeDef *UartHandle)
{
if(UartHandle.ErrorCode & (HAL_UART_ERROR_RTO)){
RXcount=UartHandle.RxXferSize-UartHandle.RxXferCount;
/* Set transmission flag: transfer complete */
UartReady = SET;
HAL_UART_Abort_IT(UartHandle);//noise on the line or wrong bytes will cause further OVR ints to
//be called after the final RTO causing havoc. END transfer here.
}
else{//maybe ovr is set
}
}