cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 toolchain for HiTop IDE

patil
Associate II
Posted on February 07, 2016 at 16:07

Hi,

I have a STM32 Performance stick based on STM32F103RBT6 microcontroller with me and I have developed a USB keyboard application using HiTop IDE with Tasking C compiler. The firmware written works well.

Now I want to test the code written for it on the  microcontroller only. But I have decided to use the relatively low cost STM32F102xx series micro, which is enough for my USB application.

But in Hitop IDE there is no other option for other microcontroller selection, I have to use the Performance stick to work with it.

Is there any STM32 toolchain avilable for HiTop IDE or do I have to use other IDE like Keil.

#toolchain #ide #!stm32
1 REPLY 1
Posted on February 07, 2016 at 18:35

Yes should discuss your support needs with Hitex directly?

There are many ARM IDE available, you need to review which ones meet your needs for pricing and support.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..