2016-02-07 7:43 AM
Hi All!
We know, what stm32f746 use ULPI whithUSB3320C-EZK to realise USB HS.
I could not run the Demonstration project and any other projects, relating to the USB HS.And I am surprised that USB3320C chip really hot, very straight.I want to ask: it must be heated or I did something with meals and it burned down.?I can add: if power the board from USB st-link, the feeling is that the board does not have enough voltage: this I see on the screen flicker, and if the processor is loaded, the screen may not light at all.Now I feed giving 5V power supply separately..It seems to me that I had somehow what is burned chip.Thanks! #stm32f746discoveryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.